Part Number: TMP423 Good morning!
I have seen that P/N TMP423AIDCNT is in EOL and I wanted to check with you if the only difference between P/N TMP423AIDCNT and TMP423AIDCNR is the packaging quantity (respectively 250 vs 3000).
Thank you.
Part Number: TMP464 Other Parts Discussed in Thread: TMP432 , , TMP423 , TMP422 , TMP422-EP Is any of these TMP432, TMP464, TMP423, TMP422, or temperature monitor available in military temp? I couldn't find any on TI website.
Part Number: TMP423 Other Parts Discussed in Thread: TMP421 I want to use TMP423 to replace TMP421.
Is it okay to connect pin3 and pin4 of TMP423 to GND? If there is a problem, please tell me the connection destination of pin3 and pin4 of TMP423.
Part Number: TMP423-Q1 Hi,
When using Vcc of 5V can the two wire interface be 3.3V? In other words pins 6 and 7 are pulled up to 3.3V through a resistor. Is the logic voltage levels of SMBus(tm), also apply then to the two wire? Is there anything else…
Part Number: TMP423 Other Parts Discussed in Thread: TMP421 , TMP422 the customer would like to install 2x TMP423 on board.
As the datasheet, the TMP421 supports nine slave device addresses and the TMP422 supports four slave device How about the TMP423…
Part Number: TMP423 Other Parts Discussed in Thread: TMP421 , TMP464 , TMP468 , TMP107 , TMP104 Hi
We use it on the base of the charging pile, the distance between the main body and the split of the charging pile is 10m, the temperature of the charging socket…
Part Number: TMP423 Hi Sir,
Could you please help to check below TMP423 schematic and TMP423 function will work well when BJT on/off?
Thanks
Schematic
Zoom in part of BTJ circuit
Part Number: TMP423 Hi,expect.
When i use TMP423(DXP1 connect with 2N3904 NPN and DXP2 connect with 2N3906 PNP),and put them in a constant environment such as 25℃,the temp reading from Remote Temp1 and Remote Remp2 will be about 2℃ different。
How can…