Part Number: TMP431 Hi Team,
Customer found they always need to use software reset firstly then they can read the remote temperature registers normally, otherwise the remote temperature registers will not change. They feel confused about it and want to…
Part Number: TMP431 Other Parts Discussed in Thread: TMP423 Hi Team,
Do we have fully P2P device w/ EMC1414-A-AIA-TR? Customer is looking for it.
Best,
Stanley
Part Number: TMP431 Other Parts Discussed in Thread: TMP390 , TMP303 Hi Team,
Customer is asking if TMP431 has the capability to alert user if temp is within a specific range? (Not beyond the limits)
So for example we make High Limit = 0C, Low Limit =…
Part Number: TMP431 Other Parts Discussed in Thread: LM95245 , TMP411 , TMP401 , TMP451 Hi Sir,
I am looking for EMC1412-A-ACZL-TR pin to pin 2nd source replacement. This is MSOP-8 package.
https://ww1.microchip.com/downloads/en/DeviceDoc/20005273A.pdf
I found…
Part Number: TMP431 Hi Team, I would like to ask about BUSY bit. 1) I understand The BUSY bit reads as 1 if the ADC is making a conversion and the bit reads as 0 if the ADC is not converting. Does BUSY bit assert "1" during "Conversion Time" that shows in Figure…
Part Number: TMP431 Hi All,
I have a question about ALERT / THERM2 for TMP431.
Please tell me when the following register settings are asserted. 【Configuration register1 MASK(7)=0 AL/TH(5)=1】
In my opinion, when using the ALERT / THERM2 terminal as THERM…
Part Number: TMP431 Hi Team,
Do we have any requirements for the impedance of traces or cables when using external transistor for measuring temperature?
Best,
Stanley
Part Number: TMP431 Hi,
if TMP431 connect FPGA internal BJT as remote sense, but the BJT spec. is higher than TI recommendation on data sheet, item 3 and 4.
1. Base-emitter voltage > 0.25 V at 6 μA, at the highest sensed temperature: OK
2. Base…
Part Number: TMP431 Hi All,
I have a question about TMP431A.
The default for the TMP431A is 85℃ It is asserted at boot time if it is already 85℃ when the device is booted. Is there a way around this?
Or is it possible to negate THERM and ALERT / THERM2…
Part Number: TMP431 Other Parts Discussed in Thread: DXP Hi Team,
If customer does not want to use pin DxP and DxN, is that okay to short DxP and DxN together? Or any other connections are suggested here? Many thanks for your help.
Best,
Stanley