Part Number: TMP432 Hello,
Our customer purchased these from franchised channel. The parts came in 13inch reels. According to public info, this should be placed on 7inch reels.
Are the reels used inter-changeably at TI?
Please check if there was a mistake…
Part Number: Hello!
I would like to use the PCA9543A I2C bus switch with a set of TMP432 temperature sensors
but have gotten confused as to how to calculate the pull up resistor values,
the decoupling capacitors and the supply voltage of PCA9543A.
I…
Part Number: TMP432 Hi Team,
Good day.
Our customer is currently using the TMP432ADGST with the MMBT3906 transistor to measure the temperature. Could you shed some light on how the temperature is linked to the transistor collector current?
The table 1…
Part Number: TMP442 Other Parts Discussed in Thread: TMP432 , DXP Hi,
TMP442 datasheet states that the series resistance Rs should be under 1K, or 300 ohm if beta-compensation is used.
Does this refer to the total series resistance of both base and emitter…
Part Number: TMP432 Hi Team,
Customer would like to know the benefits & drawbacks as he select NPN compare to PNP?
I just know from DS description that N{N need with diode connected, PNP can be transistor or diode connected.
Benefits :
Diode-connected…
Part Number: TMP432 Hello E2E,
We have a question on data hold on time.
In fast mode, the data hold time range is from 20ns as min to 900ns as max.
In customer application, they use 100kHz clock frequency as normal mode on i2c interface and the data hold…
Part Number: TMP432 Hello,
I have a question about value of bypass capacitor and pull-up resistor.
<Q1>
bypass capacitor: 0.1uF? Is 0.1mF error in writing?
<Q2>
pull up resistor: 10k-ohm? Is 10kW error in writing?
Best Regards, Kaede Kudo
…
Part Number: TMP432 Other Parts Discussed in Thread: DXP Hi Sir,
There are 2 questions need to clarify with you.
1. As below diagram, if we connect 1.8V to BJT on pin2/3/4/5, is it OK for TMP432?
2. What is the purpose for the cap in red box? Is it must…
Part Number: TMP432 Other Parts Discussed in Thread: TMP468 Customer is curious about whether there are other temp sensor solution better than TMP432. They are expecting a more compacted solution? Thank you.