Part Number: TMP442 Other Parts Discussed in Thread: TMP461EVM , TMP468EVM , TMP468 HI, in the datasheet it is no clear what the sequences of couples of current the TMP442 applied (6uA ,12uA and after 60uA, 120uA, OR 6uA,60uA and after 12uA, 120uA) to the…
Part Number: TMP442 Other Parts Discussed in Thread: TMP432 , DXP Hi,
TMP442 datasheet states that the series resistance Rs should be under 1K, or 300 ohm if beta-compensation is used.
Does this refer to the total series resistance of both base and emitter…
Part Number: TMP442 Other Parts Discussed in Thread: INA219 TMP442B cannot be found on the I2C bus via a scanning method. The 'B' version of the part should be at I2C address 0x4D but it is not seen. I2C addresses for TMP442 are set in factory…
Part Number: TMP442 Hi, Support
I have a question about the TMP442B I2C addressing. From the datasheet, the address of the TMP442B is pre factory set address. 1001101b.
So, if I want to use two TMP442B in one board, how can I address them.. there…
Part Number: TMP442 Other Parts Discussed in Thread: DXP , TMP422 Hi All,
I have a question about the TMP442.
The connection of DXP2/DXM2, which is unused, is described in the datasheet as an Open or GND connection. In E2E, it also states that DXP and DXN…
Part Number: TMP442 Other Parts Discussed in Thread: DXP Hi Team,
Would you advise how should the customer connect no using input of
TMP442?
Is it OK to open or connect to GND better?
Thanks
Best regards,
Shidara
Part Number: TMP442 Hi team,
I'm looking at the TMP442 datasheet and can't locate the ΘJB and ΘJC values. What are the values for the junction-to-board and junction-to-case resistances?
Thanks,
AH
Part Number: TMP442
Hi sir,
Could you please provide me the following thermal information,
Missing the following thermal information. Junction to board resistance Junction to case resistance
Thank you very much.
Regards,
Frank
sfgvip@126.com