Part Number: TMP451 Hello, My customer is considering ADI MAX6642 as a remote temperature sensor for Intel Arria10. TI “Cross-reference search” shows TMP451 as an alternative device. Arria10 datasheet specifies diode source current max/min = 100uA/10uA…
Part Number: TMP451 Hi TI Team,
I would like to use the THERM pin available on your sensor to trigger when local temperature goes above the -5deg celsius.
Providing that the sensor is working on "extended temperature range configuration" mode, would…
Part Number: TMP451 Other Parts Discussed in Thread: LM90 Hi team,
One of my customers is using LM90 Linux driver for TMP451, they are using hwmon bus to read temperature. it's supposed to be temp_input folder under /sys/class/hwmon path, but the folder…
Part Number: TMP451-Q1 Other Parts Discussed in Thread: TMP451 Hi, Team
My customer use TMP451 and have a question about the Alert pin as below:
1, when Temperature is higher than limit, the Alert pin is from high to Low, that is OK.
2, when the…
Part Number: TMP451-Q1
hi expert
i have some questions about setting temperature limit function by configurating related registers, such as "Local temperature high limit", "Local temperature low limit ", "Remote temperature high limit (high byte)…
Part Number: TMP422-Q1 Other Parts Discussed in Thread: TMP451-Q1 , What is the maximum rating current ((limited current) of TPM451-Q1 PIN1(V+,) PIN1~3(DX1~DX4)?
Part Number: TMP451-Q1 Hi,TI team:
For TMP451-Q1,pin6 can be used as ALERT or THERM2.What's the difference between this 2 usecaes? When used as ALERT, do there still have Hysteresis?
TMP451-Q1 already have THERM(pin4), why does it need ALERT/THERM2…
Part Number: TMP451 Other Parts Discussed in Thread: TMP411 , , Does the D+ pin bias change with VCC? I've got a thermal diode in a large package with ESD diodes that kick in above 1V, and I just wanted to make sure the TMP451 wasn't going to turn these…