Part Number: TMP461 Other Parts Discussed in Thread: TMP116
Hi, Support Team
Do we have for DDR4 Temperature sensor with integated 4Kbit EEPROM for Memory Module solution?
TMP116? TMP461?
if any suggestion, Please advise me.
Thanks,
Best regards,
La…
Part Number: TMP461 Other Parts Discussed in Thread: ADS124S08 Team,
Can TMP461 be used for other type of end sensors?
Customer is ideally looking for one IC solution that can be used with many type of sensor and that can be access digitally (I2C, SPI…
Part Number: TMP461-SP Hello,
I am working on a derating analysis per document number MDA-QS-003-PMAP-REVC (Appendix A), and wanted to know if you have more data available than what your datasheet has provided me. I am specifically inquiring the (1)…
Hi Steve,
To add to Josh's response, there is no path to V+ through SDA and SCL. This can be seen in section 6.1 of the datasheet (absolute maximum ratings), since the input voltage specifications of SCL and SDA are not dependent on V+. In situations…
Part Number: TMP461-SP Hi folks
The existing SEE report for this device does not have any information on SET (single event transients). It only addresses SEL.
https://www.ti.com/lit/pdf/sbok029
Is a more detailed test report covering SET available?
If…
Part Number: TMP461 Hi all,
I hope you are doing well. I have several questions regarding the usage of the TMP461 that I am looking for answers on:
Q1) Does the TMP461 treat the voltage developed between the D+ and the D- pins as a true differential…
Part Number: TMP461-SP Hello, I am looking at the DS for TMP461-SP and I did not see a VOH spec for THERM/THERM2. Are these known?
Also, are there specs on the driver source current ? Thank you.
Part Number: TMP461-SP Other Parts Discussed in Thread: TMP461
From page 6 of the datasheet, the data setup (t(HDDAT)) and hold time (t(SUDAT)) is defined for writes on the SMBus. I need to know what the setup and hold time will be for the read cycle…
Part Number: TMP461 Hi Team,
We would like to ask your help regarding our customer's inquiry below
When a temperature reading is negative, how are the Lower Byte supposed to be interpreted? Am I to assume it is always a positive offset? If not, then…
Part Number: TMP461 Hi Temp Sensor Folks,
Could you help me to get answer on the related thread? My customer also connects 10kohm resisor to 3.3V V+ power rail on A0 and A1 pin and the address is not properly read. What's the minimum pull-up strength…