Part Number: TMP461-SP
Hi Experts!
In space applications we typically frown on connecting signal pins directly to supply pins.
For the Address (A0 and A1) pins of the TMP461-SP what is the maximum value resistor that can be used instead of a direct connection…
Part Number: TMP461-SP We are having some testing issues with our TMP461-SP device. Debugging has lead me to need to know how the D- pin is connected in the device and if there is any ESD protection devices on it.
What is D- connected to in the device…
Part Number: TMP461-SP Is there a typo in the TMP461-SP datasheet? "Short-circuit" should be "Open-circuit".
7.3.5 SensorFault
The TMP461-SPdevice can sense a fault at the D+ input resulting from an incorrect diode connection. The…
Part Number: TMP461 Dear Sir/Madam,
I have look thru both TMP461 and TMP461-SP datasheet, both components have the same identical functional block, the different is the package.
1) I would like to find out what is the wafer technologies node for both…
Part Number: TMP461-SP Hi experts!
I'm looking for the reliability/qualification report for the TMP461-SP HKU package to address my customer's question.
"Would you please let me know if TI recommends body soldering the following device? If…
Part Number: TMP461-SP I am looking over the displacement damage report for the TMP461-SP (report SBOK034) and have a question on the temp error data shown on page 21 (attached). Per the data in the table, it appears that the Delta is much greater at…
Part Number: TMP461-SP Hello,
The TMP461-SP has a note “a report on SEU is available on request"
I’d like to request this report,
I am also interested in SEFI testing if performed.
Thank you,
Andrew
Part Number: TMP461-SP Team,
How does one change the current source low, medium, high see figure below.
The datasheet indicates 3 remove current source bands. Are these adjusted with the correction factor register or Range Bit 2?
Thank you.