Other Parts Discussed in Thread: TMP1075 , TMP468 , TMP117 , TMP461 , TMP464 , TMP139 , TMP75 HI Team,
would you have any thoughts for the possible replacement part with CAT34? I know it is not the full part number, but if you have some info please share to…
Hi Lalit,
Yes, LM95234 can be used with the TDIODE pins of ADC12DJ3200. We also offer TMP423 and TMP464 which are suitable for 3 or 4 channels.
The TCRIT pins are open drain and can be tied together to perform logical OR known as wire-OR.
All of the TCRIT…
Part Number: TMP423 Other Parts Discussed in Thread: TMP421 , TMP464 , TMP468 , TMP107 , TMP104 Hi
We use it on the base of the charging pile, the distance between the main body and the split of the charging pile is 10m, the temperature of the charging socket…
Part Number: TCA9544A Other Parts Discussed in Thread: TMP464 Hi Sirs,
We have use TCA9544A +TMP464
1. Could you help double check schematic?
2. TCA9544A INT0-3 could use one PU resistor?
Thanks!!
Schematic:
1.output~new.pdf
Part Number: TMP422 Other Parts Discussed in Thread: TMP461 , , DXP , TMP464 , TMP468 Hi,
We commonly use the TMP461 to interface with devices which only have DXP pulled out. In that case, we would connect DXN to GND. Can the TMP422 support this mode? We…
Part Number: TMP468 Other Parts Discussed in Thread: TMP464 , Hello,
Two questions in regards to TMP464/TMP468:
1. Is there any difference between the THERM and THERM2 outputs (one is supposed to be configured at a higher temp than the other, speed, etc…
Hello Toshihiro-San,
All of our remote temperature sensors will also include a local temperature sensor. Are you looking for 4 remote channels and 1 local channel? Or 3 remote channels and 1 local channel?
For 4 remote channels I would recommend the T…