Part Number: TMP468 Hi all,
Looking at the datasheet accuracy info of TMP468 we are wondering what the definition is used for typical value.
Can anybody explain which would be the correct definition for typical?
Which would be the percentage of TMP468…
Part Number: TMP468 Hello,
The TMP468 datasheet states that the assigned address depends on the ADD pin, but it does not specify when the ADD pin is actually read/strobed to determine address.
During which state is the ADD pin read to determine address…
Part Number: TMP468 Hi Team,
Please help us to get the Case Temperature (Tc) of the Part TMP468AIRGT as it is needed for the thermal simulation of our project.
Part Number: TMP468 Hello,
I would like to ask regarding D+/D- signals. I use a multilayer PCB. At layer 2 I have placed all the D+ signals as a diff pairs. On layer 3 I have placed the D- as a plane.
So my question is: Is it correct to add the D- as…
Part Number: TMP468 Hi expert,
my customer is using TMP458 as remote temp sensor, we have question about the PCB trace limitation. in the datasheet, there is only requirement for PCB width 5mil, and twisted pair cable length 8 inch. customer the max PCB…
Part Number: TMP468 Hello, I am working with a custom board that has one TMP468 Temperature Monitor installed. I have the first four Remote Temperature Monitors connected to MMBT3906-7-F for temperature measurement
Local Temperature: he78, Table 2 somewhere…
Part Number: TMP468 Hi Temp team,
I am reading an application report ——“ Optimizing Remote Diode Temperature Sensor Design (Rev. A) ”.
I have some question to a sk you for help.
In page 7 of application report, a way to reduce error…