Part Number: TMP464 Other Parts Discussed in Thread: TMP513 , TMP512 , ADS1118 , AMC80 Hi Team,
do we have temp with voltage detector together?
Thermal sensor x2, Voltage detector x4
thanks!
Other Parts Discussed in Thread: BQ77905 , BQ76920 , TMP512 , LM5056A [?] 3 in one Voltage/Current/Temperature sensor max ~20V DC
is there such sensor exist? i see one in linear technology but only up to 5.5V
Other Parts Discussed in Thread: TMP512 I am starting to use the TMP512, and have a question on the remote temp sensors... The datasheet specifies that a remote PNP transistor can be connected as a diode or with the collector grounded. What is the difference…
Hi Angela,
The only part with remote junction temperature sensors that has an EVM is the TMP512. The TMP512 has a lot of circuitry that the TMP42x parts do not have, but the remote-junction and local temperature specs are similar between the two parts…