Part Number: TMP513 I am trying to read the manufacture ID from the TMP513 through I2C fro PIC32MK0128MCA0148.
My sequence is given below.
1) Master starts communication
2) Master sends Two-Wire 7bit Slave Address
3) Master sends R/W bit low (I include…
Part Number: TMP513 Hello Team,
We use the TMP513 to get temperature data, the local temp is right, but remove temp is error with negateive data, do you have any configuration application note or reference for us.
Thanks!
Temp=39.3 -191.4 -192.5 -190…
Part Number: TMP513 Dear Josh,
I need clarification for unused ADC input pins for high-side current shunt monitor.
This part chosen based on stock availability.I can connect link configuration3,but i can not keep additional resistor on my PCB.Please confirm…
Part Number: TMP513 For the integrated temperature sensor on the TMP513, should we expect it to more closely track the ambient air temperature directly above the chip package? Or will it be closer to the copper temperature that the chip is bonded to …
Part Number: TMP513 Other Parts Discussed in Thread: LM83 , TMP423 Dear Team,
I am planning to use your product TMP513 in my module for temperature sensing purpose.I am not going to measure voltage/power/current consumption.Some dedicated pins(Vin+ and…
Part Number: TMP513 Hi Team,
I am trying to write and read from shunt positive limit register where I am seeing some junk data and on later of any write and read operation the data which is written in the shunt positive limit register is read.
When could…
Part Number: TMP513 I can see that negative current can be measured, so I assume this is okay, but I wanted to check. I'm measuring a 24V rail. Is it okay, if I connect the 24 rail supply to VIN-, and the load side of the sense resistor to VIN+? I know…
Part Number: TMP513 I saw in the related question that the QFN pad should be connected to ground. I had the same question, as it is not mentioned in the datasheet (maybe worth updating the datasheet to mention this?). Ok, so I'm connecting it to ground…