Part Number: TMP513 Hi everyone! My problem is i cannot understand, what value i need to write in , for exapmle, bus voltage positive register. I cannot find this information in datasheet and forum. According datasheet, for 32v value corresponds hexidemical…
Part Number: TMP513 Other Parts Discussed in Thread: TMP464 , TMP461 HI, team,
Just need to conform with you one question.
How to How to connect VIN+/VIN- if voltage/current sensing is not used? Just connect 2 pins to GND, or leave floating?
Thanks.
J…
Part Number: TMP513 Other Parts Discussed in Thread: INA3221 TMP513 does not show thermal pad in the pin list, and does not say anywhere in the datasheet that it can or can not be connected to, say, ground...
Is the thermal pad connected at all on the…
Part Number: TMP513 The RSA package Land Pattern Data in the datasheet indicates that there is a Route Keep Out Area by Pin 1. Can you clarify what the purpose of this is for and if it applies to the TMP513?
I did see a reference in SLUA271A for possible…
Other Parts Discussed in Thread: TMP513 HI Dan,
I have a customer planning to use (Remote sensing) external transistor for PCB board temp monitoring as diagram below showed in Datasheet.
The customer couldn’t find transistor selection recommendation from…
Other Parts Discussed in Thread: TMP513 , TMP275 , TMP112 Hi,
I used the TMP513 in my design, and currently I check the function of my products in the chamber.
I've tested at -20, -10, 0, 25 and 40 degree (V+=5V), but I found the local temp. error will be…
Other Parts Discussed in Thread: TMP513 Hi
I am using TMP513 in my design, to read the input voltage and input current with the following conditions,
Bus voltage: 12.00VDC
Input current range: 0A to 2A.
Shunt resistor: 5 mohm.
While reading the data…
Other Parts Discussed in Thread: TMP513 Does the TMP513 use an internal clock for its conversions and/or state machines? If yes, what is its frequency and how is it generated? For compliance/certification, I need to document all the different clock domains…