Part Number: TMP708 Other Parts Discussed in Thread: TMP390 , Hi Sirs,
Sorry to bother you.
Our setting as below There will turn on system at 0 degrees If we want to set 3 degrees to turn on system, how much value can be adjusted to?
Please help provide it…
Part Number: TMP708-Q1 Dear TI, I wants to receive the following materials. > Material contents We can not search on the web, so we ask for it.
Look forward to your good news soon. My email address is below. > bj.han@wtmec.com
Part Number: TMP708-Q1 Hi Team,
I have automotive customer that has application needing one low-cost temperature switch.
While promoting TMP708-Q1, I find that it's AEC-Q100 grade 1 device, with the absolute operation temperature range of -40 to 125…
Part Number: TMP708 Hello Temp Sensor experts
How to Test the TMP708 functionality at 20C - with Rset set to 100C trip point ?..
Customer needs to in the production test the functionality of the TMP708 at Ta= 20C - while having the Rset mounted and set…
Part Number: TMP708 Other Parts Discussed in Thread: TMP303 , LM57 Hi team,
My customer wants to use the TMP708, but they want to set the Trip point=0°, so based on the hysteresis=10°, so the OT=1 triger point is -10°.
But you know the device…
Part Number: TMP708 Hi everybody,
one of our customers uses the TMP708AIDBVR to detect an over temperature case at 105°C. He had some problems with the stability/precision.
He added a cap at the SET pin and everything was fine.. After that he removed…
Other Parts Discussed in Thread: TMP708 hi,
I'm using the TMP708 in my design.
I have set the threshold to around 108oC with 9.53k resistor.
however, when I test the circuit with a heat-gun and thermocouple, the device trips at case temperature of…
Other Parts Discussed in Thread: LM57 We need to setting threshold at 125° , But , Calculate rule is Error (-1.46 K) , Pls help to comment How to setting temperature threshold at 125° , thanks!
Other Parts Discussed in Thread: TMP708 Please let me questions in TMP708.
When Rset resistance is not connected to the SET terminal, what will be output to the OT # terminal?
(If the SET terminal of OPEN!)
Best regards