Part Number: TMP75 Other Parts Discussed in Thread: TMP175 , , TMP1075 Hi TI service team,
I have one question about TMP75/TMP175 temperature sensor accuracy (operation temperature: -25 degree to 85 degree, specification need within +/-2 degree) like…
Part Number: TMP461EVM Other Parts Discussed in Thread: TMP75 Tool/software: Hello
I'm trying to use the TMP461EVM, but when I try and run the software I always get the same error message "SM-USB-DIG API TMP75.lvlib:Merge Error.vi" regardless of if…
Part Number: TMP75 Tool/software: Hi Team,
Our customer is using TMP75 in their application and encountered an issue described below.
We used the TMP75 temp sensors for project its its reads sometimes more than two bytes & its causing us to temp…
Part Number: TMP75 Other Parts Discussed in Thread: LM339 , Hello,
Some TI devices, such as LM339, give a maximum "case temperature" spec in the datasheet. I do not see an equivalent spec for TMP75. Can you please let me know the maximum case temperature…
Part Number: TMP75-Q1 Other Parts Discussed in Thread: TMP75 Tool/software: Hi team,
As per the datasheet of TMP75, the max operating temperature is -55℃ to 127℃. And the accuracy is +/-3℃ from -40℃ to 125℃.
Could you please confirm what the accuracy…
Part Number: TMP75 I am trying to read temperature data by communicating between TMP75 and microcontroller.
Start condition → slave address → pointer register (temperature register) → restart → slave address → data byte 1 → data byte 2
By communicating…
Part Number: TMP75 Other Parts Discussed in Thread: TMP1075 Hello,
I performed a register read for register 0xF (which is not mentioned in the datasheet) and found that it contains the value 7500. This is the same value that the TMP1075 datasheet…
Part Number: TMP75
From they layout guild says ground plane , does it mean that the layer closest to the Temp Sensor needs to be laid with a ground plane, or should I just hollow out all the wiring layers under the IC? Thank you.
Part Number: TMP75 Hi expert,
Customer has a production product used TMP75 and forgot to mount pull high/low resistor on the board of address pins.
So far didn't see any issues but wondering what would be the status of address pin if floating? We…
Part Number: TMP75 Other Parts Discussed in Thread: TMP1075 Hi team,
my customer want to seek a solution with the smaller PCB size or package size.
the interface should be still I2C and the accuracy and the other functions should be at a similar level…