Part Number: TMP75B-Q1 Other Parts Discussed in Thread: TMP75-Q1 , TMP75C-Q1 Tool/software:
Hi, expert
The URL for TMP75B-Q1 states that it is equipped with an I2C/SMBus interface, but the datasheet refers to it as a "two-wire" interface, and…
Part Number: TMP75C-Q1 Other Parts Discussed in Thread: TMP75 , TMP75C Tool/software: I'm using TMP75 to measure PCB temperature and it's accurate when the device is in open air but when the pcb is in its plastic enclosure and is fully potted its now…
Part Number: TMP75C Other Parts Discussed in Thread: TMP114 Hi Team,
Can you let me know if we have a smaller size analog temp sensor that can replace TMP75C/NCT75/ADT75? Customer application is RRH/MMU in communication equipment. They usually use supply…
Part Number: TMP75C Hi Temperature Sensor team,
Are there any of the PINs below that can be configured for SI attributes? (Or is it a fixed pin that can't be set as a user?) If so, please inquire which register you can set it through.
Device…
Part Number: TMP75C Hi Sensors team,
I`m Taemin who is FAE in Korea.
My customer uses TMP75C, however customer board can not meet T(hddat) specification 0~900ns.
The measured data is 1.3 us on customer board with FAST MODE(SCL 100kHz setup).
In…
Part Number: TMP75C Other Parts Discussed in Thread: TMP75 , TMP175 Dear E2E support team
This question is about linux device driver for TMP75C temperature sensor.
I'm considering implementation the TMP75C temperature sensor on the Linux system which…
Part Number: TMP75C Hi Team,
Customer will read the temperature register in every 1s. But the problem is that the register is updated in every 80ms in continuous mode so there would be an overlap every 4s - customer's system will read the register value…
Part Number: TMP75C Hello Team,
Customer is using TMP75CIDGKR and wondering if ALERT pin being pulled-up to 1.8V while VS is 3.3V. Datasheet mentions "Vs or higher but up to 3.6V". Does it mean that a voltage lower than Vs is not acceptable?
Part Number: TMP75C Other Parts Discussed in Thread: TMP1075 Hello,
May I know MFR ID / MODEL / REVISION register values? (0x99~0x9B) What value should be read from those registers? I cannot see the information in datasheet. Thanks!
Part Number: TMP75C Other Parts Discussed in Thread: TMP75 , TMP1075 Hi Team,
Is there a "Device ID" field inside the TMP75C registers that allows an micro-controller to distinguish between it and TMP75?
Thanks!
Roy