Other Parts Discussed in Thread: CONTROLSUITE , TMDSDOCK28335 , TMDSHVMTRINSPIN , TMS320C28343 Is Delfino C28343 controlCARD compatible with TMDSDOCK28335 and TMDSHVMTRINSPIN? Can I port motor control applications provided by controlSuite to TMS320C28343 ? …
Hello,
I received my TMS320C28343 Experimenter kit, but there is no 5V power supply (mentioned in the getting started overview)? Is it normal? Can I use the USB connector JP2 has the power supply (with SW1 in USB position)?
Another point, I did not succeed…
Other Parts Discussed in Thread: TMS320C28343 Hi,I have TMS320C28343 and I can't connect it with the Code Composer Studio because TMS320C28343 is not on the list of available factory boards in CCS.
I have CCS Platinum v3.3.
Can you help me?
This information is in the datasheet for the TMS320C28343 device found on the Product Folder .
Look in the Electrical Specifications section for items #1, #2, #3 and Thermal/Mechanical Data section for items #4, #5, #6.
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Other Parts Discussed in Thread: TMS320C28343 Hi,
I am using a C2000 XDS510LC probe connected over USB for debugging a TMS320C28343 based boad (experimenter kit) under CCS4 (latest version) and everything works fine there.
Also, if I run SDConfigEx utility…
Other Parts Discussed in Thread: TMS320C28343 Hello,
I am hoping someone can help me with an issue I am having while booting a TMS320C28343 from external flash via SPI. For some reason when I include operations such as atan2() or others located in <math…
Other Parts Discussed in Thread: TMS320C28346 , TMS320C28343 I'm trying to use SDFlash to load a program onto my TMS320C28346's EEPROM. The algo that comes with SDFlash supports a C28346, but with the EEPROM AT49BV802D.
I can't seem to find any…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…