Part Number: TMS320C28346 Hi expert,
Can C28346 support method to identify Hardware reset and power-on reset?
End customer is concerning about the HARDWARE_RESET and power on about customer's module.
BR
Emma
Part Number: TMS320C28346 Hi,
when I press the debug buttion (green bug button) in CCS 6(while the compiler version is V5.2.8), there seems that boot28.inc can not be found, the message shows"Can't find a source file at "/sim/sds12/scratch/jnash_rtsbuild_dflcmp2510…
Part Number: TMS320C28346 Hello,
I would like to configure the use of the eQEP to detect a falling edge in stand of a rising edge.
I looked at
TMS320x2834x Delfino Enhanced Quadrature Encoder Pulse (eQEP) Module Reference Guide
and found QDECCTL.XCR writing…
Part Number: TMS320C28346 Hello,
My customer has a question for XCLKIN input waveform of C28346 to confirm if it is no problem. I want to send the waveform in separated email. Could you please assign someone?
Regards, Oba
Part Number: TMS320C28346 Hello. I'm working with Tms320c28346.
And, I use spi-a boot with flash-memory.
I'd like to make user bootloader.
But i don't have concept about bootloader.
Could you provide me information about this?
Thanks.
…
Part Number: TMS320C28346 Hi Team,
From TMS320x2834x Delfino Boot ROM Reference Guide, it list the part of SPI EEPROM as below which all are very small, question is if SPI boot can support 512KB or bigger SPI EEPROM or flash? any suggestion about this…
Part Number: TMS320C28346 Hi Team,
My customer want to use TI C28346 to connect one parallel NOR Flash (1 M x 16bits), one parallel SRAM (1 M x 16bits) and internally set McBSP-A inputs in DMA mode. they plan to use XINTF Zone6 (XZCS6/) for parallel NOR…
The above did not resolve my problem, as I felt the "older version" approach could be a rabbit hole.
But, it did cause me to flip to the Debug Server Scripting (DSS) scripting interface to automate execution of a .out file we created that is…
Part Number: TMS320C28346 Hello team,
Hope you are doing well. When you get a chance can you share some feedback on below question on TMS320C28346 :
are 1501 and 1531 date codes. What is the shelf life of this part and can we use them if they are re-b…