Part Number: TMS320C6201 Hi Team,
We would like to ask your help regarding our customer's inquiry below.
1. We need compiler support or suggestions for compiler to be used for building files existing TMS320C6201 controller. 2. In our existing architecture…
Part Number: TMS320C6201 Hi:
We are looking for a solution for AC3 decoder, according to the document " implementation of AC-3 decoder on tms320c62x ", that TMS320C62x series chips can implement AC-3 decoding.
There are several questions about…
Part Number: TMS320C6201 1) I am facing issue with csl header files i downloaded from your forum and installed it after that header file issue got resolved and i am stuck with another error kindly help .
i am not able to use CACHE_getL1PSize(); and CACHE_getL2Size…
Part Number: TMS320C6201 Hi -
I am being asked to perform a Destructive Physical Analysis on this part: TMS320C6201GJCA200. Can you please let me know if this part uses gold wire bonds, copper wire bonds, or is a flip chip.
Thank you,
Cameron
Part Number: TMS320C6201
Tool/software: Code Composer Studio
We are trying to move away from an old setup using Windows XP, CCS 2.0 to continue supporting a product using the C6201. We would like to use Windows 10 and the newest CCS possible that still…
Part Number: TMS320C6655 Other Parts Discussed in Thread: TMS320C6201 , Hi,
We had used TMS320C6201 in our earlier project and it has 32-bit EMIF with Max Freq of 200 MHZ .
At Present,We are using TMS320C6655 and it has a 16 Bit EMIF with frequency of Max…
Hello Charles,
I am worried about using DSPs (①TMS320C30/31/33 or ②TMS320C54x or ③ TMS320C6201) instead of Tiva MCU for THS1206 interface.
However, I am afraid that I have not studied DSPs.
Because I had time and effort to study Tiva MCU.
Q3> Which is…
Hello,
I want to interface the Ti ADC THS1260 device to the MCU.
However, interface (①TMS320C30/31/33 or ②TMS320C54x or ③ TMS320C6201) of THS1260 attached below.
I received the source code using GPIO mode as the MSP430 device for the Parallel External…
Part Number: TMS320C6415 Other Parts Discussed in Thread: TMS320C6201 , 66AK2G12 Hi,
Do TI have a DSP & Software that can perform echo canceler on 2 T1 links.
Please advise.
Thanks
Part Number: TMS320C6657 Other Parts Discussed in Thread: SN74AVC16T245 , SN74V245 , TMS320C6201 Tool/software: TI-RTOS Hello
I would like to ask for advice regarding a design. The question contains some elements of software and some elements of hardware…