Chen,
yes, I have experimented the GPIO interrupt and GPIO-interrupt latency....
Measured the clock cycles between the GPIO interrupt occurrence to the GPIO ISR ( Interrupt service routine).
For me, it takes, 210 CPU cycles.
Total no of CPU cycles…
Part Number: TMS320C6657 Other Parts Discussed in Thread: LM10011
Hi TI E2E experts,
I want to assemble TMS320C6657 1.25GHz on my design that has TMS320C6657 1GHz.
1. As I understand from the datasheet, TMS320C6657 1GHz Vs 1.25GHz are full-pin compatible…
Part Number: TMS320C6657 Dear TI
We are using a design looks preety much a like the C6657 EVM except that there is an extra DDR3 chip for ECC.
There 512Mb in the DDR3 area in our design (the address map for teh SDRAM is: 0x80 000 000 - 0x82 000 000.
…
HI,
If you are successful running the EDMA PING PONG test as per the FAQ, I posted above, then, why do you need the other tests?
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1242663/faq-tms320c6678-how-to-create-a-edma-ping…
Part Number: TMS320C6657 Hi,
Can you please provide some information and reference for how to calculate the address ranges? I can't unfortunately not find any reference for how to calculate the ECC ranges using the register
An example:
CSL_EMIF4F_SetECCAddressRange…
Part Number: TMS320C6657 Hello
I am using two EVM's (TMS320c6657) communicating using PCIE.
I was able to read and write using EDMA in both sizes, now I want to test write using cpu.
write from root complex to endpoint : OK but i couldn't write the…
Part Number: TMS320C6657 Other Parts Discussed in Thread: MATHLIB Hi,
I have imported DSP_add16_66_LE_ELF project from this C:\ti\dsplib_c66x_3_4_0_4\packages\ti\dsplib\src\DSP_add16\c66\DSP_add16_66_LE_ELF. when I am building this project, i am getting…
Doron,
As per the functional block diagram of McBSP of C6657, the data transmission happens through the the EDMA transfer controllers.
So, the sample code is provided with EDMA.
"There is one EDMA Channel Controller on the C665x device: EDMA3_CC. It has…