MDK said: Just to clarify - the TMS320C6655 and C6657 are "Active" devices but you do not provide any support for them?
Yes, devices that can be bought on ti.com if they are listed as "Active". The software support for these is provided as…
Part Number: TMS320C6657 Other Parts Discussed in Thread: TMDSEVM6657 , UCD9222 , UCD7242 Team,
Asking on behalf of my customer.
Customer is seeing unexpected variations in power consumption of the TMS320C6657 in their design. Measurements have been made…
Alex,
To build the platform library, please follow the steps given here. ( Especially the video steps)
[FAQ] TMS320C6657: How to build and run the platform test on C6657 EVM ? - Processors forum - Processors - TI E2E support forums
---
If you come across…
Kevin Parker said: I already posted a screenshot of "C6000-Linker properties"--> Include options taken after performing the steps in 'How to resolve cerrno in Platform Test Example in TI-RTOS SDK'. Please refer to the first post of this…
Part Number: TMS320C6657 Other Parts Discussed in Thread: TMS320C6655 Hi
Subject: failed on connection to the evaluation board
I am using TMS320C66x Evaluation module I am trying to connect to the evaluation board in the
Code Composer Studio Version:…
Part Number: TMS320C6657 Hi Team,
Can you please help with below questions:
My customer is working towards getting our DSP(TMS320CC6657) to boot from SPI NOR flash upon power on:
I currently am running into a couple of issues as I work through a guide…
Part Number: TMS320C6655 Other Parts Discussed in Thread: TMS320C6657 Hi TI E2E experts,
TMS320C6655 and TMS320C6657 are full-pin compatible?
As for the electrical design should I consider more parameters, such as power consumption differences between…
Part Number: TMS320C6657 I have modified the default GEL file to initialize DDR3 memory and PLL1 and PLL2. When debugging in no boot mode there are no issues. However when booting from SPI NOR Flash, the DSP successfully boots ( this is confirmed by LED…
Part Number: TMS320C6657
Hi DSP Champs
Is there no more new line-up of DSPs? Will also Keystone series continue to be produced?
Also What CPU series can replace tms320c6657?
Thanks.
Regards,
Jack