Other Parts Discussed in Thread: TMS320C6671 Hello,
I am in trouble with connecting DSPs to MCU,
Actually I planed to connect three DSPs to MCU over SPI first, but found that DSPs support only master mode and don't support multiple master mode.
The…
Other Parts Discussed in Thread: TMS320C6671 While creating a new target configuration for a TMS320C6671 I notice that TI's default configuration shows two cores in the device. See image below. I'm wondering why...the 6671 is a single core device or am…
Other Parts Discussed in Thread: TMS320C6671 Hi,
Do TMS320C6671/72/74/78 pin to pin compatible?
Is there any document describing the migration between TMS320C6671/72/74/78?
Regards.
Other Parts Discussed in Thread: TMS320C6671 For one of our projects, we are looking at the processor TMS320C6671 as one of the solution. But I need two dissimilar compilers for the code cross compilation to the target to comply with the dissimilarity requirement…
Other Parts Discussed in Thread: TMS320C6671 One of my customers is planning to use the TMS320C6671 in their design. They are asking the following questions.
will the XDS510usb work with keystone devices?
do we need to use a 60 pin jtag header?
does…
Waseem,
I would take a look at the C667x devices including TMS320C6670 and TMS320C6671 to get started.
These feature more than 512KB of on-chip memory along with a floating-point DSP.
Regards,
Kyle
Other Parts Discussed in Thread: 66AK2H06 , 66AK2H12 , 66AK2H14 , EVMK2EX , 66AK2E05 , TMDSEVM6657 , TMS320C6657 , TMS320C6655 , TMS320C6654 , TMDSEVM6678 , TMS320C6678 , TMS320C6674 , TMS320C6671 , TMS320C6672 Hi,
Please provide the list of SDK available for the Keystone…
Other Parts Discussed in Thread: TMS320C6671TMS320C6671 is missing as a 'Device Name' from the New RTSC Platform wizard in CCSv5. How do I get it added?
Thanks.
Hi Nate,
Thanks for the advice! I followed your instructions, and it doesn't seem to be an SDK or package problem. When I rebuild, I still get the following console output:
**** Clean-only build of configuration Debug for project odsdemo_16xx_dss…
Hi Nitin,
Thank you for the reply.
With the help of migration document, i am able to port from xwr1642 to xwr6843, but when I try to build the dss, I get an error.
Kindly find the attachment file for error log.
Thanks and regards,
Vijaya Krishna.
…