Part Number: TMS320C6745 Other Parts Discussed in Thread: OMAP-L137 , DP83640 , Using the evaluation board "OMAP-L137", we achieved an ethernet sustainable rate of 30 Mbps, far from the theoretical maximum of 100 Mbps. Can it be due to limitations of the…
Part Number: TMS320C6745 Hi,
there is a strange implementation in uart_v0.c in the pdk.
In case of error, the interrupt callback calls a function to manage the error:
static void UART_v0_hwiIntFxn(uintptr_t arg) { UART_Handle handle = (UART_Handle)ar…
Part Number: TMS320C6745 Other Parts Discussed in Thread: SYSBIOS In my project i need to restart the cpu.
Why this?
I use NDK and the user of the system can change:
- IP
- Gateway
- Ports
- Active service
The fastest and secure way to do this for me is…
Part Number: TMS320C6745 Hi, i am using TMS320C6745.
I am seeing that most of functions of the official C674x dsplib are quite "general purpose", in the sense that they are compiled under few operating hypothesis. In particular, the batch size N is often…
Part Number: TMS320C6745 Tool/software: Code Composer Studio i tried simulating tms6745 using ccs5.4, but i found that the assembler is of 6200, which is fixed point dsp.
how do i simulate floating point 6745 using ccs5.4
Part Number: TMS320C6745 Other Parts Discussed in Thread: SYSBIOS Tool/software: Code Composer Studio Hello
i'm developing on a C6745 DSP an application and i need to use 2 MCASP hardware modules (MCASP0, MCASP1) to receive/transmit 8+8 mono channels.…
Part Number: TMS320C6745 Using pdk 1_0_10
The library provided use this to obtain the MAC address for NDK.
int32_t nimu_get_emac_info(uint32_t port_num, NIMU_EMAC_EXT_info * emac_info) { uint32_t mac_addr2, mac_addr1;
emac_info->port_num = port_num;…
Part Number: TMS320C6745 We need the uart for communication between processors.
The uart must be FULL DUPLEX and must be able to receive packets with an unknown length (in other words the dsp must be always in RX and get all the incoming bytes).
Pdk for…