Part Number: TMS320DM6435
Tool/software: TI C/C++ Compiler
Hello
I have the problem to build a main project including some libraries and one of them (pf_drv_dm6435xp_eabi) is program-level optimized and have a file with another build option.
If I build…
Other Parts Discussed in Thread: TMS320DM6435 Hi, I'm working with a TMS320DM6435 where an exception occurs. My task is to debug errors which occur on retoured camera sensors from the customer. This sensor serie already runs a few years so this error should…
Other Parts Discussed in Thread: TMS320DM6437 , TMS320DM6435 I have a question about an apparent discrepancy between the crystal clock input option defined in the TMS320DM6435 spec (SPRS344C, June 2008) and the reference design TMS320DM6437 Evaluation Module…
Vivek Srinivasan said: We are having a compiler error while compiling our source code for the below platform.
CPU
o DaVinci ( TMS320DM6435 )
Tool chain:
o external (TI CGTOOLS 7.4.16 for C6000) in Cygwin environment
I can repeat the error with that combination…
Other Parts Discussed in Thread: TMS320DM6435 Hello DSP team,
I have a question from a company actively using the TMS320DM6435 in their design. Since the part has gone NRND what are the risks of continuing to ship this product and future products based…
No, you can configure that GPIO as general purpose IO after reset.
You can refer to the following DM6435 data sheet, page no 52, table 2-25.
www.ti.com/.../tms320dm6435.pdf
For proper DM6435 device operation, this pin must be pulled up via an external…
Hello,
Please refer section 2.8 Device and Development-Support Tool Nomenclature in device datasheet to know the description of each legend in the part number.
www.ti.com/.../tms320dm6435.pdf
The ZWT6 refers to ZWT package with device speed of 600MHz…
Other Parts Discussed in Thread: TMS320DM6435 The following code seems to be producing a non-initialized array:
int num = 3;
int * vals = new int[num]();
If I understand it correctly, according to C++98 5.3.4.15 (expr.new) and 8.5.5 (dcl.init), it should…