Other Parts Discussed in Thread: TMS320DM647 Hi,All
I have some problems with my platform of DM648.According to the EVMDM648 I designed my own PCB,but the Ethernet does't work!I try to run the example of climet.pjt with NDK 2.0.0 and try to ping my…
Other Parts Discussed in Thread: TMS320DM647 Team,
a) The " Using the TMS320DM647/DM648 Bootloader - SPRAAJ1D " app note does speak about an optional .cfg file that can be used. However there are no specific format described.
- Can we assume that…
Hi,
For REFCLKP/N clock rate the possible suggested is either 50MHz or 62.5MHz or 125MHz, and the corresponding Line Rate is 625Mbps or 1250Mbps.
TMS320DM647/DM648 DSP 3 Port Switch Ethernet Subsystem User's Guide (Rev. B) http://www.ti.com/lit/ug…
Other Parts Discussed in Thread: TMS320DM648 , TMS320DM647 Hi all,
The local agent give us two type of DM648, TMS320DM648ZUTD1 and TMS320DM648ZUTD9;
What's the differences of them?
Where do I find the differences in TI Web?
Thanks…
Hi Yury, Please refer to the data sheet of DM647, chapter 6.4 and 6.4.1 www.ti.com/.../tms320dm647.pdf SYSCLK4 is used as the EMIFA AECLKOUT [When SYSCLK4 is used as the EMIF input clock source, the actual clock goes through a divider and the frequency…
Other Parts Discussed in Thread: DM3730 , TMS320DM647 , OMAP3530 I am using a LogicPd DM3730 Torpedo Development kit with a Spectrum Digital XDS510 USB with Code Composer v5.1 with Sys/Bios 6.33.02.31. I have been using CCSv3.3 with this target without issues…
Hi David,
Thanks for you information. I didn't use the NDK but I already got it working. It works fine except in promisc mode,
and I don't have the latest am387x documents, I took TMS320DM647/DM648 DSP 3PSW user guide as a reference.
If you…
Lee,
As I mentioned above in this thread:
When you are want to set/change the state in MDSTAT register, you need to follow the procedure/steps explained in section 6.4 in TMS320DM647 /DM648 DSP Subsystem User's Guide ( http://www.ti.com/litv/pdf/s…
Other Parts Discussed in Thread: TMS320DM647 We are using mpeg4 encoder
Id:MP4VENC_TI Ver:1.21.005 Released by:DEV_100_V_MPEG4_E_1_21_005 Built:Feb 24 2009 05:36:04
In the supplied app/Client/Test/Src/TestAppEncoder.c there are the following comment…
Other Parts Discussed in Thread: TMS320DM647 Hello
I am reading the document , TMS320DM647/DM648 DSP 3 Port Switch (3PSW) Ethernet Subsystem.
There are few terms that I have no idea , can anyone please elaborate :
Flow _ Thresh
CFI
VLAN tag
VLAN ID…