Part Number: TMS320DM8147 Tool/software: Linux Hi, all
My platform is DM8127, rdk is rdk3.8.0.
When I configure the sensor output bt1120 data to dm8127.
where i need to configure to tell the data is bt1120?
Part Number: TMS320DM8147 Hi
USB0_DRVVBUS, when enabling the VBUS charge pump, will be driven as a active high signal from the Processor DM8147. Is there any way that we can make this signal active low, when enabling the VBUS charge pump?
Thanks and Re…
Part Number: TMS320DM8147 Hi
I have two main queries listed below:
1. Is it necessary to stick with the AS length and skew requirements given in datasheet Table 8-75? Is it ok if we length exceeds to 200mils, then the required 100 mils.
2. Is there any…
Part Number: TMS320DM8147 Hi,
I have a requirement to drive two leds from Serial ATA disk 0 Activity LED output of DM8147 Processor.
Will this pin have required drive strength to drive two LEDs, or should I consider using a buffer? Please let me know the…
Part Number: TMS320DM8147 Hi
We have a requirement to interface 2GByte DDR3 to DM8147 Processsor,
We have planned to connect 2x4Gbit DDR3 to each bank.
In datasheet, it is mentioned as "Memory device capacity: 64Mb, 128Mb, 256Mb, 512Mb, 1Gb, 2Gb, and…
Part Number: TMS320DM8147
Hi,
We have planned to use 2GB eMMC Flash as a boot device for DM8147 Processor in for one of our new requiement.
We will be using 8 bi transfer mode. We do not have any reference design with eMMC Flash device.
Please let us…
Part Number: TMS320DM8147 Tool/software: Linux Hello TI,
How many Video streams of data can i encode in parallel on DM8147 Processor. Is this support available in software. Do i need the HDVPSS package to do this.
What are the resolutions that are supported…
Part Number: TMS320DM8147 Tool/software: Linux Hello,
I am referring to the following page:
1. However, PSP 04.07.00.02 Supports 2.6.37. I wanted to check if TI814X is supported in newer kernels Such as 3.xx or 4.xx Kernels.
2. Also, Which PSP is the…
Part Number: TMS320DM8147 Other Parts Discussed in Thread: TVP5158 , TVP7002 Hi
We have a requirement to interface 4 channels of 8 bit YCbCr data inputs from Video decoder to DM8147 Processor. Please find attached block diagram of our required implementation…
Part Number: TMS320DM8147 Tool/software: Linux Hello
I understand that the question is very newbie
please could you help me
I have TMS320DM8147 device and I have 8107-toolchains, cgt_a8
could you please say how to prebuild a linux like a ubuntu ur debian…