Part Number: TMS320F2800155-Q1 Other Parts Discussed in Thread: C2000WARE Hi TI Team,
I do not find any information in the data sheet regarding the conversion function (how many Voltage or ADC counts per °C) and the offset of the internal temperature…
Part Number: TMS320F2800155-Q1 Issue Description: After configuring Secure Boot, flashing the .out file followed by the .hex file, the program fails to execute. Detailed Secure Boot configuration can be found in the attached dcsm.asm file. The hex utility…
Part Number: TMS320F2800155-Q1 hi
i wanted to know that what should be the excution time for adc
adcStruct[AIP_IP1].adc_buffer = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER0);
i am calling this in ISR ..which is triggered by EPWM trigger..
…
Part Number: TMS320F2800155-Q1 Hi,
I had to configure Bootpins for high but we forgot in hardware and we gave it pull down..
we want the pin to be pull down only...
I dont understand How to do that From TRM
Kindly guide me through the steps for…
Hello,
zhang tao said: Why is it that when using the emulator for debugging, the encryption is successful and the code can run
Did you perform an ECSL or CSM unlock when running the application with the DCSM enabled? If you only do a ECSL unlock,…
Part Number: TMS320F2800155-Q1 When I was using single-byte reading, the program suddenly crashed. After further investigation, I found this issue here. I would like to ask if this semicolon is written incorrectly?
And why is it that when performing…
Part Number: TMS320F2800155-Q1 Hi
I am working on a project where I need to implement a bootloader that can load application code via CAN on a TI microcontroller. I am completely new to bootloader development and would appreciate guidance on how to…
Part Number: TMS320F2800155-Q1 Our program is stored in RAM during runtime, while the program itself is stored in Flash. Additionally, the relevant definitions for initialization in the boot section and the APP section are stored in the common RAM. We…
Part Number: TMS320F2800155-Q1 Tool/software: Dear Team:
1、How CAN I tell if the CAN bus is busoff?
2、When the bus is BUSOFF, how can I get the bus to recover?
Best Wishs
Zhang
Part Number: TMS320F2800155-Q1 Other Parts Discussed in Thread: C2000WARE Tool/software: Dear team:
I would like to ask you something. In the process of upgrading bootleader, I first need to download Flash Drive to RAM.And then download my app.
Is…