Part Number: TMS320F280023 It can work on RAM.
On Flash, encountered below errors:
Can't find a source file at "..\src\IQNsinPU.asm" Locate the file or edit the source lookup path to include its location.
--
Thanks & Regards
Part Number: TMS320F280023 Hi
When debugging the device in Code Composer Studio, I cannot get the device to flash past sector 7 (0x.
I have updated the .cml file to include sector 8 - see Image 1 attached
When editing the debug configuration settings…
Part Number: TMS320F280023 Other Parts Discussed in Thread: C2000WARE Hi
i am hitesh. i'm working with TMS320F280023 microcontroller. I have a problem debugging the program, my code build sucesfully but not working in debugging mode
C28xx_CPU1: Error…
Part Number: TMS320F280023 Hi Experts,
Nice to talk with you. Customer is using F280023 for OBC/DCDC application.
When CJTAG is used in the project, there is a issue occur like below, could you give us suggestion for this case? Thanks.
Schematic:
…
Hi Linda,
The command line interface for projects support creating new projects and importing/building existing ones. You cannot modify the properties of an existing one from the command line (at least not easily).
Thanks
ki
Part Number: TMS320F280023 Hi team,
Here's an issue from the customer may need your help:
Finished building target: "mega_afci_text.out" Building secondary target: "mega_afci_text.hex" Invoking: C2000 Hex Utility "C:/soft_f/CCS_v12…
Part Number: TMS320F280023 Other Parts Discussed in Thread: TIDM-1022 , TIDA-010062 Dears:
Customer want to design 1600W communication power supply -- topological structure: single-phase bridge PFC+LLC (half bridge). Is there source code support?
Part Number: TMS320F280023 I tried to synchronize the ECAP1 input by the output of the EPwm1SYNCOUT signal.
In the datasheet there is a register SYNCSELECT described to select the ECAP1SYNCIN bit.
But unfortunately I cannot find the TRIG_REGS Register…
Hi Andreas, I have filed an internal issue to resolve this and will get back to you once a resolution is arrived at. Closing this thread for the time being.
Regards, Pawan
Part Number: TMS320F280023 HI team,
We are facing ADC samples read problem in TMS320f280023 controller Please find the Adc Configration details below :
We are triggering ADC on EPWM . Initaillay if i apply the break point and check adc sampling counts…