Part Number: TMS320F280025C Other Parts Discussed in Thread: C2000WARE Dear sir/mam
i am working on uart/sci . i am using SCIwritechararray function .this function is able to transmite string and char value but it is not transmitting integer value or hexa…
Part Number: TMS320F280025C Im working in C2000 MCU along with drv8343 here the motor current ( Idq_in_A) varies when i give pressure to the pump externally.
1. If Idq_in_A is the motor current means i want to maintain the motor current constant while giving…
Can you have a look at the datasheet of the DRV8343 and check if there is any fault pin triggered by the over current? If yes, you need to change the current limitation value of the DRV8343.
Part Number: TMS320F280025C Hi,
Would like know if my application mainly for MOTOR CONTROL (based on universal_motorcontrol_lab_f28002x) can I use 280025 instead of 280025C ?
Danny
Part Number: TMS320F280025C Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hi All,
I'm using c2000ware SDK and TMS320F280025C MCU. Configured HRPWM via sysconfig and added all relevant features include dead-band settings The problem is : when…
Part Number: TMS320F280025C How to merge two application hex files using hex2000 utility?
or do you know any utility which supports word addressing and can be used to merge two application hex files.
Part Number: TMS320F280025C Other Parts Discussed in Thread: SYSCONFIG Hello.
After updating CCS, the following warning message appeared from a project that was created and built before the update. What should I do to get rid of this caution message?
Thank…
Part Number: TMS320F280025C Other Parts Discussed in Thread: SYSCONFIG Hi, I'm trying to set specific dead band
working on HRPWM mode so dead band clock *2 rate system clock = 10 ns (100 MHz) I want to set FED = 90nSec, so calculated the following DBFED…
Part Number: TMS320F280025C Hello,
I am using TMS320F280025C for my project. The current design does not have an external crystal oscillator (XTAL). In the TRM, on page 573, there is a note stating "The CAN boot loader uses XTAL as the bit clock source…
Part Number: TMS320F280025C Hello. Please forgive my poor English notation.
I am using the ePWM function of the TMS320F280025C to generate PWM waves with variable duty ratio. So, is it possible to disable the B side (EPWMxB) when all I want to use is the…