Part Number: TMS320F280025C Other Parts Discussed in Thread: TIDM-02010 , C2000WARE , Dear TI Support Team,
I am currently working with the C2000Ware MotorControl SDK (version 5.04.00.00), specifically the TIDM-02010 DMPFC solution for F28002x devices…
Part Number: TMS320F280025C Iam working with TMS320F280025C + DRV8343 running the BLDC motor at DMC LEVEL 4 using INSTA SPIN FOC, I could find fluctuation in the waveform when the torque of the motor increasing.
Part Number: TMS320F280025C Iam using TMS320F280025C + DRV8343.
Inputs entered in coding is based on the motor parameters.
1.I want to increase the torque to 6 Nm.
what parameter should i tune to increase the torque?
Part Number: TMS320F280025C Other Parts Discussed in Thread: LVSERVOMTR , C2000WARE Tool/software: I'm developing with TMSM320F280025C and DRV8323RH kit on LVSERVOMTR, and in different build levels, it could always read status and outputs from DRV8323RH…
Part Number: TMS320F280025C Other Parts Discussed in Thread: C2000WARE Dear sir/mam
i am working on uart/sci . i am using SCIwritechararray function .this function is able to transmite string and char value but it is not transmitting integer value or…
Part Number: TMS320F280025C Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello everyone,
I'm working on a project with the TMS320F280025C controller where I need to transfer ADC data to a DAC6551 via SPI communication. However, I'm…
Part Number: TMS320F280025C-Q1 Hi, experts,
My customer plans to use 3rd party programer to flash C2000 devices. He tried to generate HEX file through C2000 HEX Unitily in CCS, to make sure no content missing in generated HEX file, he has to set "romwidth…
Part Number: TMS320F280025C Other Parts Discussed in Thread: SYSCONFIG I set up the CAN peripheral using SYSconfig. 500k, 2 object 1 transmit, one receive. I have a test message transmitting with each trasnition of the "life" LED about every second. If…
Part Number: TMS320F280025C Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi guys, I have a bit of a problem with canbus message transferring exploiting tx interrupt line. The problem is the following: I setup the mailbox to be 8 byte…
Part Number: TMS320F280025C Tool/software: I congfig TI PMBUS as slave mode.
When PMBUS master sends an address that does not match slave address, I want to know:
1. Will PMBSTS.SLAVE_ADDR_READY of PMBUS slave be set to 1?
2. Will PMBHSA of PMBUS…