Part Number: TMS320F280037-Q1 Other Parts Discussed in Thread: TPS653860-Q1 Tool/software: We are using this uC, whats the recommended PMIC? we need 5V, 3.3V and 3.3V. Vin from 6 to 36V. I have TPS653860-Q1 considered, but has too many output rails and…
Part Number: TMS320F280037
Tool/software:
Hello,
I have a modified .cmd file that has MEMORY and SECTIONS as shown below.
I have no errors when I build the code, but the .stack section does not get added to the memory map file and the xml file…
Part Number: TMS320F280037 Tool/software: I have been trying to follow the command line instructions on TI's site - I have an existing project which builds OK using CCS 20.1.1. If I try importing this project into a new workspace created from the command…
Part Number: TMS320F280037 Other Parts Discussed in Thread: C2000WARE Tool/software: Dear Engineers. Good Morning. I am developing the RTOS for TMS320F280037 MCU. However I am seeking help from the downloaded example from the TI website. The problem which…
Part Number: TMS320F280037
Tool/software:
I am running MISRA 2012 compliance on a motor project we are doing and have found that the code provided as example in the motorcontrolsdk seems to violate MISRA 11.8. For example: motorVars_M1 is defined…
Part Number: TMS320F280037 Tool/software: I am using pins shared by ADC and SDFM for both SD clock and data fed by 10MHz AMC1303 signals. This seems to be causing noise on ADC conversions on other analog pins. Since the AMC1303 drives its own clock free…
Part Number: TMS320F280037 Tool/software: Hi champs,
I am asking this for our customer.
The user want to enable these modules when needed and disable them when not needed.
1. If the user wants to disable EPWM+ADC+DMA
Can they just use these…
Part Number: TMS320F280037 Tool/software: Hi Experts,
My customer uses DMA 1ch to deliver ADC result to buffer. ADCA : 3ea(result 0,1,2) ADCB : 3ea(result 0,1,2)
ADCA result 0,1,2 and ADCB result 0,1 are normally transferred to buffer, but ADCB result…
Part Number: TMS320F280037 Other Parts Discussed in Thread: SYSCONFIG Hi,
I am using a external crystal OSC at 16MHz. Previously develop with Launchxl 39C, I modify the project to our board using a F280037 with a 16MHz (instead of 20MHz from launchXL…
Part Number: TMS320F280037 Tool/software: I was recently having trouble with using serial flash programming due to a memory map being generated with a code section that wasn't aligned to 8 words. It was one of two sections included in a group that used…