Part Number: TMS320F280038C-Q1 Tool/software: Hello,
since the existing CCS will be discontinued and the newer Theia version should be used instead for the C2000 development, we started to evaluate it and found out that the continuous refresh interval in…
Hi Vamsi,
Vamsi Gudivada said: Regarding the verification error: It is not from flash erase/program. It is from standalone verification of the memory against the file that you provided. Are you sure the same file is programmed on to the device previously…
Part Number: TMS320F280038C-Q1 Tool/software: We are configuring epwm3 and epwm4 channels with exactly the same configuration as follows:
- both on up counter mode
- both with TBPRD = 999 (for T=8.33us)
- both with CMPA = 499
- SyncOut of ePWM3 is SycnIn…
Part Number: TMS320F280038C-Q1 Tool/software: Team,
A customer of mine is trying to communicate with a SPI device which is expecting 24 bit data. As this is not directly supported, they are sending 3x 8 bit data. SPI is in FIFO mode.
In rare cases it…
Part Number: TMS320F280038C-Q1 Hi,
I use EPWM to trigger ADC. Therefore, I go in to interrupt at every 20usec by using below line.
Can I update number 2 to 1 or 2 to 3 during my main-loop? How and when does the change takes place in real? Can you draw…
Part Number: TMS320F280038C-Q1 Other Parts Discussed in Thread: C2000WARE Hi Champs,
Customer works on an OBC , USB debugger sometimes crashes because of noises. Therefore they are using modbus protocol over UART/RS485 (SCI) for real time debugging. This…
Part Number: TMS320F280038C-Q1 Other Parts Discussed in Thread: C2000WARE Hi,
I am trying to use interrupt utilizing ePWM1.
I checked the interrupt cycle (frequency) by using one GPIO OUTPUT in the interrupt function (High -> Low).
It was set to have…
Part Number: TMS320F280038C-Q1 Hi,
In my application, I'm using PCMC control configuration on CMPSS1 High comparator and a protection on CMPSS1 Low comparator. During program running, with an external command on CANBUS, I need to change CMPSS1 Low comparator…
Part Number: TMS320F280038C-Q1 Hi,
1) For F28003x devices, can I write some parameters and values to unused flash banks, or to some sectors during my program executing real-time? If it is impossible with F28003x devices , can you offer alterative part numbers…
Part Number: TMS320F280038C-Q1 Trouble Reading Register ST1: (Error -1156 @ 0x6) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry…