Part Number: TMS320F280039C Other Parts Discussed in Thread: C2000WARE Hello, I configred the GPIO9 to the ePWM TRIP5 through the configration below:
EALLOW;
GpioCtrlRegs.GPAQSEL1.bit.GPIO9 = 3;
InputXbarRegs.INPUT2SELECT = 9;
EPwmXbarRegs.TRIP5MUX0TO15CFG…
Ok, that all makes sense and explains the behavior that I am seeing. Sounds like the approach I am using of keeping it in repeat mode and disabling the interrupts when I don't want to feed more data is the best we can do. The last bit is always 0 for…
Part Number: TMS320F280039C Other Parts Discussed in Thread: SYSCONFIG Hi TI Team
I am trying to read AC volts through ADC on my TMS320F280039C, my AC volts input comes from output of my op-amp and i can see my sine wave and i have set 1.65 V DC offset…
Part Number: TMS320F280039C Dear Champs,
I am asking this for our customer.
The user wants to generate a random number from a set.
For example, to pick up a random number from integer 1 to 1000.
This is running from C28x.
1. Does F28003x have any HW…
Part Number: TMS320F280039C Other Parts Discussed in Thread: ADS7038 Hi, I am using ADS7038 and TMS39C controller for reading 7 analog signals.
The YELLOW highlighted pins are getting high unwantedly.
ADS7038 SPI initialization function: void SPI_init()…
Part Number: TMS320F280039C Other Parts Discussed in Thread: SYSCONFIG , , C2000WARE Hi,
I have developed an application for the TMS320F280039C. Because I use FreeRTOS, I have built on the SDK example with SysConfig. Now, however, I would like to freeze…
Part Number: TMS320F280039C Other Parts Discussed in Thread: UNIFLASH , CCSTUDIO , I'm trying to set up a CI system for F280039 based board. Is there any standard Docker image for building C2000 firmware? I've found a few different files out there but…
Part Number: TMS320F280039C Hi Team,
1. Our current topology is a three-phase out-of-phase LLC. If we do not use the SFO library to calculate the MEP scale factor, can the frequency, duty cycle and phase be updated correctly?
2. If you define MEP yourself…
Part Number: TMS320F280039C Hi
I am migrating the code from F2808 to F280039C. When working on F2808, we were using the code security password to protect the MCU from unauthorized firmware upload. On F280039C, I saw there is a dual code security module…