Part Number: TMS320F280040-Q1
Hello,
Try to enable the EPWM1 interrupt and config as below in syscfg tool:
ISR is as this:
void INT_myEPWM1_ISR(void)
{
int i = 0;
i++;
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}
If the breakpoint…
Hi Crane,
Crane Shao said: At the same time, any ideas on the cause of the different results from ADC-B15 and ADC-A1?
Can you confirm that this testing was done with nothing else connected to the board besides power and the ADC input (i.e. no toggling GPIO…
Crane Shao said: I try to configure Cppcheck as an external tool in Eclipse. It seems that there is no "External tools" under Run in the main menu. Is it taken out of CCS or I just didn't find it?
CCS hides it by default. To re-enable it…
Part Number: TMS320F280040-Q1 Hello:
What are the digitally controlled Reference designs we can look into with very high-efficiency topologies: such as inteleaved LLC?
Appreciate any direction for such information.
-r
Part Number: TMS320F280040-Q1 Hi,
Trip-Zone input timing
What does Pulse duration mean in following PWM Hi-Z Characteristics in datasheet?
Is the timing required to trigger the fault condition on the ePWM module?
If yes, the waveform is not understandable…
Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: SYSCONFIG Hello,
I tried to use the example "buffdac_ex1_enable" on LaunchPad Piccolo. And measure the output on J7 - Pin 70 and 62. It is always 0.
I tried to modify the analog reference…
Crane Shao said: Probably the TCB is already corrupted when the overflow hook is called.
Yes, that could be the reason CCS is not able to map the value to a valid ASCII character.
Crane Shao said: But when the program is running not from JTAG, it works…