Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: UNIFLASH Hello,
Actually I downloaded it before, but couldn't find it any more from googling it.
Not available at this page:
https://www.ti.com/tool/TMDSEMU110-U#order-start-developmen…
Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: SYSCONFIG Hello,
When the phase shift between PWM channels PWM1 and PWM2 is changing when the program is running, the synchronization between two PWM channels gets lost, which means the phase…
Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: UNIFLASH Hello,
Is there is JTAG programming software, which is separated from CCS?
I am using the one that is integrated with CCS. However, in some cases, I need a separate one to do just…
Crane Shao said: Now I want to delete the linked resources and go back to the original status. How to do that?
What do you mean by "go back to original status"? Do you mean deleting the link to the sysconfig file and having it physically added back to…
Part Number: TMS320F280040-Q1 Hi Team,
Our customer is using three TMS320F28004 microcontrollers in their design. He would like to explore the option of using CAN internal to their circuit board ( not using a CAN transceiver) to communicate between the…
Part Number: TMS320F280040-Q1 Hello,
I am using ADC and would like to know the accuracy that can be achieved.
I didn't take any special measurements and the accuracy I got is around 10%. Is this the typical accuracy, or kind of low?
Thanks!
Crane …
Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: C2000WARE
Hello,
I am using the function I2CBusScan() to scan the I2C device FRAM MB85RC1MT.
The slave addresses I got are 0x52, 0x53, 0x7C. But from the specification of this memory IC, the…
Part Number: TMS320F280040-Q1 Other Parts Discussed in Thread: SYSCONFIG Hello,
I want to set ePWM1A as the trigger for ADCA Ch6 and do the change as below and the register value is correct.
And I checked the ePWM1A and its output is correct.
But, the…
Part Number: TMS320F280040-Q1 Hello,
When I look at the dead-band waveforms, I see two waveforms for each setting.
For the AHC option, there are two waveforms. The above one shows RED and the below one shows FED. Do you know why there are shown in two…
Crane Shao said: how to cancel that event to have normal PWM output?
So you clear the latch for OST to remove the condition. The way to do it is writing a 1 to TZCLR[OST] which is EPWM_clearTripZone flag function in the table above. They are both in the…