Part Number: TMS320F280048-Q1 Dear TI Team,
Getting from the Mahindra & Mahindra, we are facing the problem on MCU " F280048PMQR" from one of our OBC (on board charger) supplier, For Vehicle on board charging application.
The particular MCU 8D report…
Part Number: TMS320F280048-Q1 Tool/software: Hi, experts,
I am asking this question on behave of my customer.
Customers are using the TMS320F280048 chip on their products. During the product development phase, they carried out stress tests of FLASH…
Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: C2000WARE Hi,
In my PSFB converter, I'm trying to implement oversampling on ADC B3 and ADC B6 channel. I want to do in following way. I showed figure in below.
Can you help on designing…
Part Number: TMS320F280048-Q1 Hi,
I saw some kind of usage of __attribute__(()) in some reference software. I'm trying to understand what they are and what their help is.
1) What does it to do writing __attribute__((ramfunc)) on the line before writing…
Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: C2000WARE Hi experts,
Do have static codes test on the C2000Ware driverlib and corresponding reports? Customer used driverlib in their project, and requests for the static codes test report…
Part Number: TMS320F280048-Q1 Hi,
After implementing DCL to my current working software on flash, it is required to reload the program to flash after re-energising my board. That means I always need to re-load program to flash again, after powering…
Part Number: TMS320F280048-Q1 Other Parts Discussed in Thread: C2000WARE Hello Experts,
For those flash programming, I one used code from example " flashapi_ex1_program_autoecc.c" from C2000Ware . There is one function (Fapi_doVerify)applied as:
…
Gokhan G. said: I can capture waveform at the ADCpin, which is also a CMPSS input. I can remove 1B Vgs signal and put the ADCInput signal if it is required?
Yes, that would be great.
Gokhan G. said: I also use analog to digital conversion at same…
Part Number: TMS320F280048-Q1 Hi,
In my board, I connected GPIO24 and GPIO32 to 3.3V with pull-up resistors as you can see below. It represents that device default boot mode is FLASH.
However, these pins are also can be configured as EPWM8A-8B…
Hi,
Gokhan G. said: 1) Which method do you offer to change PWM configuration after init? Do I need to write new configuration to registers at ISR or a task that is called at 1msec? Which is safe and flexible to achieve?
Typically, it is expected that…