Karthik,
I am closing this post since your application is working after copying to the Blinky template.
If you have further questions, please open a new post (since I will be OOO and may not be able to monitor this post).
Thanks and regards,
Vamsi
Part Number: TMS320F280048C Out project is using an F280048C which has a VCU unit. I am using the VCU to calculate a CRC32 checksum by calling the library routine "get_CRC32_cpu". I would like to calculate the same checksum on a windows PC to verify the…
Part Number: TMS320F280048C-Q1 Other Parts Discussed in Thread: C2000WARE Hi,
This is a continuation of the support case " ">e2e.ti.com/.../3851239 . As per the closure of the case, we were able to flash the device. However on further notice…
Part Number: TMS320F280048C-Q1 Other Parts Discussed in Thread: C2000WARE Hi Team,
My customer is evaluating F280049C Launchpad for one the applications and need to use peripherals like SPI-A, SPI-B, SCI-A, SCI-B etc along with some preprocessing and control…
Part Number: TMS320F280048C-Q1 Other Parts Discussed in Thread: ADS8900B , C2000WARE
Hi all,
I am using ADS8900B ADC to digitize a high frequency signal (< 250 KHz) at the rate of 1MSPS (or 500 KSPS) throughput with F280048C. The 1 MSPS interrupt is generated…
Part Number: TMS320F280048C Is the source code for the F28004x SCI Boot ROM code published? If so where can I find it?
We have GPIO24 (boot 0) tied to GPIO28 (SciARx). The SCiARx and SciATx lines are brought out to a connector. We ground SciARx to force…
Part Number: TMS320F280048C Tool/software: Code Composer Studio I am using an F28004x_Launchpad Development Kit to develop software for our application. I now have our own hardware with an F280048C microprocessor. I can program our 48C with our application…
Part Number: TMS320F280048C
Hi Team, I have got a doubt while designing with F280048CPMQR. 1) I am using the internal DC-DC regulator for 1.2V generation, my doubt is do I need to connect all the VDD pin externally?. or are they connected internally. Some…
Part Number: TMS320F280048C Tool/software: Code Composer Studio I am developing code to interface with an AD7988 using SPI. I have it working in the CPU. I would like to mode the code to CLA. Can anyone point me to an example that shows how to configure…
Part Number: TMS320F280048C Hello,
My customer are finalizing their schematic. We give 2 options for the FLT1 and FLT2 pins: either leave unconnected or pull-down to Vss through 4.7 kohms.
Are there any tradeoffs between these possibilities?
Thank you…