Here is what our architect suggested:
// Function returns F32 remainder of a/b
float return_float_remainder ( float a, float b) {
float value;
float i, f, retval;
/* Assign the value we will calculate the modf of */
value = a/b; // Do a floating…
Part Number: TMS320F280049 Hi, I want to connect the xds100 on a running F280049. I can connect to the target but the execution stops and I have to Resume the execution. How can I connect to the target without stopping execution?
Regards, Holger
Part Number: TMS320F280049 Hi, is the crystal oscillator stopped during a reset? And has to come up even after a warm reset? Customer is doing a warm reset (watchdog reset) and sometimes the oscillator didn't come up.
Regards, Holger
Part Number: TMS320F280049C Other Parts Discussed in Thread: TMS320F280049 Hi,
If CLB is not used, can user replace TMS320F280049 to TMS320F280049C without any change?
Thanks.
Part Number: TMS320F280049 Other Parts Discussed in Thread: CONTROLSUITE Hi Ti support team, I try to use controlSUIT, and from ABC_DQ0_POS_F.h, i have follow line:
//*********** Function Declarations *******// void ABC_DQ0_POS_F_init(ABC_DQ0_POS_F *v)…
Part Number: TMS320F280049 Other Parts Discussed in Thread: SYSCONFIG , C2000WARE Hi All,
I have a question regarding data ending up into the .hex file.
I started from the example empty_sysconfig_100pz within the C2000Ware library (v05.01.00.00). Then, I…
Part Number: TMS320F280049 Hello,
for some calculations in my project I need to work with complex numbers. I am working in CCS Version: 11.0.0.00012 with the compiler TI v 21.6.0.LTS1. The microcontroller F280049 has a CPU-Clock of 96 MHz.
Using the header…
Part Number: TMS320F280049 Hi,
for your information: in the documentation for the Flash-API spnu628a i can read: " The DCSM OTP programming must be aligned to 128-bit address boundaries and each 128-bit word may only be programmed once " So programming…
Part Number: TMS320F280049 Hello,
I have a system with 2 microcontrollers, one TMS5701227 and the other TMS320F280049. I am developing some firmware and I was using 2 JTAG debuggers, the XDS110 for the hercules, and the XDS100V3 for the C2000. We have…
Part Number: TMS320F280049 Hi, TI experts,
the PID parallel form DCL_runPID() function has both antiwindup and saturation function, what about the DF22 format, what if it saturates?
Thanks!
Shengnan