Part Number: TMS320F280049C-Q1 Hello,
There is a question about reading and writing data from CpuToCla1MsgRAM.
What would happen during reading and writing a 32bits data combined with word#1 and word#2?
The CPU writes word #1 but right when the CPU finishes…
Part Number: TMS320F280049C-Q1 Hi Champ,
From datasheet , the maximum input voltage is -0.3V to 4.6V.
Customer want to know for below input signal case , any risk that this GPIO pin will be damaged?
Maximum 4.67V, minimum is -1.12V, the overshoot time…
Part Number: TMS320F280049C-Q1 Dear champs,
I am asking this for our customer.
The user wants to implement 2-phase interleaved boost with peak current mode and slope compensation.
Can the user use PWM4A/PWM5A and CMP1/CMP2 ((PWM4A(SYNCO)=>CMP1(RAMP…
Part Number: TMS320F280049C-Q1 I'm currently building a board around the TMS320F280049C-Q1 and I'm looking for a reference hardware design for the JTAG header using the compact TI 20-pin.
This is using the XDS110 debug probe. The compact TI 20…
Part Number: TMS320F280049C-Q1 Other Parts Discussed in Thread: TMS320F280049C , TLIN1021DEVM , SYSCONFIG Hi Champs,
Customer uses TI - LAUNCHXL -F280049C (TMS320F280049C)
For the particular series they are implementing the LIN/SCI Slave driver. While testing…
Part Number: TMS320F280049C-Q1 Hello TI-Support Team,
the LIN is running in slave mode and I have been using the information from the posts:
Link 1
Link 2
to set the IDSLAVEBYTE; RXMASK and TXMASK with this calculation:
Only the ID 0x1 and 0x2 should…
Part Number: TMS320F280049C-Q1 Other Parts Discussed in Thread: TMS320F280049C , TMS320F280039C Dear TI expert,
At my project, TI C2000 TMS320F280049C is used to control the digital power supply.
The output voltage will feedback into C2000 internal…
sagar yadav1 said: Inject a fixed current on d-axis to force the rotor align to the zero angle position.-- Can you elaborate on the same
You can find the example code in the lab. Just insert the a current on the d-axis, and set the angle to zero for i-park…
Trey German8 said: I'm trying to put together a library I can hand to people so they can write custom code for my device.
Why must it be a single library? It is very common for a single project to link with multiple libraries.
The command ...
ar2000…