Part Number: TMS320F2801 Hello Champs,
F2801 board has been running for many days but currently error has been found out that the voltage of ADCREFM pin (1.43V) is higher than ADCREFP pin (1.3V).
After changing the 2.2uF Tan capacitors connected in these…
Part Number: TMS320F2801 Tool/software: Code Composer Studio Hello,
I am intending to use some TMS320F28x processor (haven't decided yet) and I would like to know if it will work on CCS V5.5 with the XDS110 JTAG Probe.
In the DS of the XDS110 I saw…
Part Number: TMS320F2808 Other Parts Discussed in Thread: TMS320F2801 Hi experts,
I am not able to find examples codes for the tms320f2808 in c2000 package whereas it is showing tms320f2801,02,03,04,05,06,07.
please help me how to use examples codes…
Lance Laliberte said: are there any triggers or situations that can cause this to happen?
None have been identified.
Lance Laliberte said: is this a hard stop of transmission meaning it will not restart transmit once stopped?
Correct. Hard stop.
Here are…
I have another repeating XRS pulse output from the processor problem. This processor was programmed and running but we detected a problem with our power supply not putting out our 20V and +/-15V supply voltages properly so we replaced the transformer…
Ganesh,
I want to clarify the device you are using. In the subject line you have listed TMS320 C 2801 which is ROM only device, https://www.ti.com/product/TMS320C2801 so there will be no flash. Do you have a TMS320 F 2801 https://www.ti.com/product/TMS32…
Other Parts Discussed in Thread: TMS320F2801 Hi All
According to the Data Manual of the TMS320F2801, transmission rate for the master and slave are different than each other(one of them is LPSCLK/4 and the other is LPSCLK/8 ), however in the SPI reference…
Hi Caglar,
The best data I can find for the F280x device will be from the website below, which has MTBF and FIT estimation for TI parts.
https://www.ti.com/quality/docs/estimator.tsp?OPN=TMS320F2801PZQ&CPN=&partNumber=TMS320F2801#resultstable …
Other Parts Discussed in Thread: TMS320F2801 , TMS320F2808 Hey everybody,
I am using microcontroller
TMS320F2801 in welding inverter. It communicates with front panel through
CAN interface.
Some processors communicate well,
some just sometimes.…