Part Number: TMS320F280200 Tool/software: Code Composer Studio Hello,
When i write to the flash of the microcontroller via visual basic then my program code got hang and a file is open indicating no source available for 0x3ff5f5. In debugging mode…
Part Number: TMS320F280200 Tool/software: Code Composer Studio Hello,
When i write to the flash of the microcontroller via visual basic then my program code got hang and a file is open indicating no source available for 0x3ff5f5. In debugging mode…
Hello Gautam,
Thank you for your reply, I will double check it on the control suite,
I haven't fully explored the control suite files yet. But anyway, thanks.
Jake
Other Parts Discussed in Thread: TMS320F280200 , CONTROLSUITE We are trying to program TMS320F280200 based board and getting the following message.
C28xx: Flash Programmer: Error encountered when writing to flash memory C28xx: File Loader: Memory write…
Other Parts Discussed in Thread: TMS320F280200 Hi,
I am working on Solar MPPT project with TMS320F280200 MCU and want to fix the address of a variable in memory but couldn't able to do it because CCS compiler is giving me warning saying : The Location…
Hi, I tried all combinations possible to generate High Resolution PWM (HRPWM) but it is not working. I am using 280200 controller with 40MHz clock. 200KHz freq PWM. Library used is SFO_TI_Build_V6b.lib.
Attaching code here, can you please let me know where…
Other Parts Discussed in Thread: TMS320F280200 Just to be sure is there any way to swp the output of the PWM after the dead band module on the tms320F280200 (i.e. sans HRPWM). I need to do a active high complementary with the active high part on an output…
Got it. Pull up controlSUITE and go to Libraries | Utilities - Flash API | Folders | F2802x Flash API
Use the 2802x_FlashAPI_BootROMSymbols_v2.01.lib and that will work.
I do get the following warnings:
warning #16002-D: build attribute vendor section…
Yuan,
I believe that the designation of Piccolo-EL in this case is a typo(we have let the document/kit owner know about it). This is referring broadly to the TMS320F280200 device, however, there is not a controlCARD for that device.
The listing for all…
Hi Sal,
Actually it seems that this library I mentioned above (( http://www.ti.com/tool/iec60730swpackages ) is more applicable since IEC-60730 is exactly what I'm looking for. But that is not my question.. I know that the F28075 is up to the task.…