Part Number: TMS320F28023 Hello Gurus:
Is there a 1/2 precision (16bit) floating point library for the 280x series of micro controllers?
I have 32 bit (float and double) routines, and also 64 bit (long double.)
Thanks, Mark.
Part Number: TMS320F28023 Tool/software: TI C/C++ Compiler Win7 32bit, CCS 6.2, F28023.
I have one statement in my C code, thus....
MUTE_OFF;
in a header file I have the following definition...
#define MUTE_OFF GpioDataRegs…
Part Number: TMS320F28023 Tool/software: Code Composer Studio Win7 32bit, CCS 6.2, F28023.
In project settings, under CCS Build -> C2000 Linker, I see a the summary of flags set; and near the -m I see a constant -m"Piccolo.map" (my project is named Piccolo…
Part Number: TMS320F28023 Tool/software: TI C/C++ Compiler I have the following code snippit:
void To523(float param_dec, uint16* param_hex) {
long param223;
long param227;
#define one_23 0x800000
#define one_27 0x8000000
param223 = param_dec * (1L…
Part Number: TMS320F28023 Tool/software: Code Composer Studio Win7 32bit, CCS 6.2, F28023.
I have tried to create some key bindings, and it really seems to be hit or miss (mostly miss) as to whether they work or not.
For example, I'd like to set ctrl…
Part Number: TMS320F28023
Tool/software: Code Composer Studio
Win7(SP1) 32 bit, CCS 6.2, F28023
As I type some words are misspelled and under lined.
In help, I found General->Editors->Text Editors->Spelling, and can change some things.
I pointed…
Part Number: TMS320F28023 Tool/software: TI C/C++ Compiler Win7 32bit F28023 (Piccolo) CCS V6 and V8
This post
https://e2e.ti.com/support/tools/ccs/f/81/p/820303/3035965#3035965
Mentions a disconnect between the compiler version and CCS version I hadn…
Part Number: TMS320F28023 Other Parts Discussed in Thread: CONTROLSUITE , C2000WARE Tool/software: TI C/C++ Compiler Win7 (32bit) CCS 8.2, F28023
I am wanting to use the on chip FLASH via the TI API.
I have an older version of controlSUITE (v3.4.9 - March…
Part Number: TMS320F28023 Tool/software: TI C/C++ Compiler Win7 32bit (SP1), CCS 6.2.0.00050, F28023.
I have been attempting to make a coefficient generator using double precision floating point (64bit) math.
I finally figured out you need to define each…
Part Number: TMS320F28023 Tool/software: Code Composer Studio Win7 32bit, CCS 6.2, F28023.
I am attempting to temporarily eliminate the run-time support library to try to find a module I have that is including library functions I don't want (like printf…