Dave Hunson said: Q1: what is a purpose of having these functions ?
This is to enable running multiple background functions in different threads at different time instances depending on use case. TI example has used in minimally for demo purpose, but a…
hi dear Luo you mentioned " using method in controlSUIET. "
Q1:what method do you mean?
Q2: please tell me where can I find that method?
regards.
Dave.
Yanming Luo said: using method in controlSUIET.
Hi Adam,
As you suggested, we will likely use the DRV8305-Q1 since it is automotive rated. It also has the TMS320F28027F-Q1 MCU onboard: http://www.ti.com/tool/DRV8305-Q1EVM so no plug-in MCU module is required. (4.4 V to 45 V, 25 A) If we can get the DRV8353RS…
Dear Luo ,
dear Luo, all I need is to set current value to have fault in higher value
for example our inverter can support 10kw motor and we connect it to 7.5kw motor so we want to set current fault to 17A (considering motor voltage is 380V ) . in this…
Part Number: TMS320F28027F
Hi Everyone,
I have implemented Lab 4 using hvkit_rev1p1 . Using gMotorVars.Iq_RefA Current Loop Control(torque) and the desired RPM(8500) is achieved!!
In that whatever acceleration i have achieved that is not enough for me…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: , TMS320F28027F Dear ALL
Pls help suggest to me , Customer is need to know Input current wavefom of DRV8305-Q1EVM .
Thank you so much & Bestregard
Prarinya
Part Number: TMS320F28027F Other Parts Discussed in Thread: TCAN1042-Q1 Hi All,
Is it possible to interface the TMS320F28027F MCU with TCAN1042-Q1 to create a CAN interface with the TMS320F28027F device?
- Leo
Part Number: TIDA-01168 Other Parts Discussed in Thread: TMS320F28027F , LM5170 , , LM5170-Q1
Hello,
im currently working on an bidiretional converter 12/48V 3KW 4phases. Im using the LM5170 as inner current loop compensator and want to use the TMS320F28027F…
Part Number: TMS320F28027F Dear Champs,
Q1: InstaSpin provide a good way of identifying motor parameter, I would like to use this for compressor(air conditional system). In most cases, the compressor is assembled in system already, that means the compressor…
Part Number: TMS320F28027F Other Parts Discussed in Thread: BQ76PL455A-Q1 Tool/software: Code Composer Studio I am using c2000 (28027F) piccolo launchpad . When i run echoback example from control suite without any changes it is running , but it takes…