Part Number: TMS320F28031 Hi team,
We are trying to support customer to run HVPSFB demo code on F28031.
Since the ADC conversion F28031 is slower than F28027, the control loop cannot run at 100kHz.
Thus, we are trying to slow down the control loop to…
Part Number: TMS320F28031 Dear Ti,
My project is to generate 220V 50Hz inverter output From varing 350V-600V Input Supply.
For this i am Using "SVGEN_MF" for This Purpose. I have implemented a Equation in the Program to Maintain 220V 50Hz Inverter…
Part Number: TMS320F28031
Tool/software: Code Composer Studio
Hi everyone,
I am using _IQ library for some of our calculations in the firmware. But I need to remove the IQ format for certain variables to make them simple integers to do some calculations…
Part Number: TMS320F28031 Hi, I am trying to get the ECAN0INTA interrupt enabled for reception and then service it with the ECAN0INTA_ISR function which is a part of the DSP2803x_DefaultIsr.c file. Here are the steps that I have followed:
Step 1 : Configuring…
Part Number: TMS320F28031
I'm seeing a large amount of overshoot and undershoot on the UART Tx line using GPIO29 on TMS320F28031.
Is there a way to reduce the drive strength in software?
If not, what would be the best way to do so in hardware?
Part Number: LAUNCHXL-F28379D Hi Experts,
In the dual axis drive project, While running the speed control loop, what is the right way to limit torque?
Can we just adjust the pi_iq loop saturation limits (Umax and Umin)?-Can you please confirm this?
…
Part Number: TMS320F28031 Other Parts Discussed in Thread: TEST2 Hi Champs,
My customer wants to use AIO as GPIO to detect the digital inputs. There are 8 switches on DIP switch, and 6 AIOs are connected to DIP switch as follows. And 1 switch is connected…
Part Number: TMS320F28031 Tool/software: Code Composer Studio why the include option don't work as the project provided by TI,
My customers' project is like this, we can't open the includes,
we hope they can like this, which has a plus and…