Part Number: TMS320F28032 Tool/software: Code Composer Studio HI,
I'M a FAE in TI, now my customer has a question.
The background is, they are trying to achieve interleave buck with TMS320F28032, buck worked in DCM mode, frequency change, and the…
Part Number: TMS320F28032 Hi Experts,
Board: F28032
CCS: CCSv3.3
Apart from the JTAG real-time emulation, can we see what mode the chip is in, is there another way to see what state the chip is in? Is the chip in emulation mode, or is it viewed…
Part Number: TMS320F28032 Hi,
I wonder do we have suggested baud rate upper limit for SCI module.
Since increase baud rate will increase the %error, do you know what's fasted baud rate you see the customer is using?
Or could you please provide the…
Part Number: TMS320F28032 Hi team,
I am supporting my customer on their F28032 project. On their PP board, the solder the chip first and then program. When they try to program the chip, they found about 1/3 of the board's MOSFET would be destoried.…
Part Number: TMS320F28032 Other Parts Discussed in Thread: C2000WARE Hi Experts,
Now the customer is having a strange problem, the F28032 chip has been working well, however the power-on is not working properly now. The reason for the initial positioning…
Part Number: TMS320F28032 Tool/software: Code Composer Studio Hi,
My customer was developing a DCDC with 28032,
After running in high temp for 7 hours, we found we can't communicate with 28032, and we found the flash was empty!!
we never saw it…
I'm really a bit desperate after this day...
I really do not get why the XDS110 thinks that the device is in reset ?
As you can see in the first image, which I posted yesterday: Reset line is going from high to low. Twice.
Also, another thing: …
Part Number: TMS320F28032 Hi Team,
Customer reported an test phenomenon: the IIC SDA/SCL PIN received voltage level of 0 to -0.64V signal which last for 176ns; and for -0.3V to -0.64V, the signal last for 80ns; but the datasheet of TMS320F28032 didn…
Part Number: TMS320F28032
Hi,
my customer would like to control 5 LEDs at 500kHz switching frequency.
The PWM frequency is 40kHz for power stage. And the main interrupt is 40kHz.
So if they add a interrupt at 500kHz dedicated for turning on and…