Part Number: TMS320F28054M Hi team,
Here's an issue from the customer may need your help:
1) with 28054 for position control, the customer only has 28069 demo board, so uses 28069 for parametric identification. Then use the drv8301kit_revD> f2805xM…
Part Number: TMS320F28054M Dear experts,
The customer requires a heavy load during the motor start-up, but does not allow the motor to rotate during the initial position phase. They thought that the instaSPIN-FOC needed to be rotated a certain angle…
Part Number: TMS320F28054M Hi! Hope that you can shed some light onto the problem we are currently having with TMS320F28054M + DRV8323S based boards. We had a working design and simply ordered a new batch of boards. New boards didn't worked. After comparing…
Part Number: TMDXCNCD28055ISO Other Parts Discussed in Thread: TMS320F28054M , , MOTORWARE Hello ALL,
Can I put a TMS320F28054M MCU on the TMDXCNCD28055ISO controlCARD and use it to run the MotorWare labs on hvkit_rev1p1hvkit_rev1p1 development kit…
I haven’t heard back from you for a week, I’m assuming you were able to resolve your issue. If not, just post a reply below (or create a new thread if the thread has locked due to time-out). Thanks.
Part Number: TMS320F28054M Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio After installing motorware, when I clicked on it, I got attached picture, can somebody tell what might have gone wrong? Also, in CCS in view -> Resource…
Part Number: TMS320F28054M Other Parts Discussed in Thread: C2000WARE Does someone know if it is possible to perform FLASH reprogramming through SCI-A bootloader or one can only load some code to RAM that way?
Part Number: TMS320F28054M Other Parts Discussed in Thread: MOTORWARE Hello,
We have a custom design based on the TMS320F28054M that runs one type of 3 phase induction motor just fine. The engineer that designed and implemented this setup is no longer…
Part Number: TMS320F28054M I have a custom f28054m board for motor control. Things are working fine, however during startup, the motor sometimes wobbles little back and forth a bit (2 to 3 degrees) before starting normally. I observed on CRO and found…
Hi Mika,
The formula should be correct to calculate the inertia based on motor parameters, but you need to use the same USER_IQ_FULL_SCALE_CURRENT_A, USER_IQ_FULL_SCALE_FREQ_Hz.. in formula as using in identification.