Part Number: TMS320F28062F Hi,
When a malfunction occurs in a noise test, the MCU cannot be reset even if the reset pin of the MCU is set to low level from the outside in order to recover from it.
If it is normal (before it malfunctions due to noise)…
Part Number: TMS320F28062F Hello TI:
I use TI's official positionless arithmetic library to drive a motor. The actual effect is that the motor does not run. The angle value output by the estimator is always 0. However, I have actually enabled the forced…
Part Number: TMS320F28062F Other Parts Discussed in Thread: CONTROLSUITE I have successfully used the ROM bootloader on the F28062 to boot from SCI. I've seen forum topics describing methods of jumping directly to the SCI_Boot function in ROM using software…
Part Number: TMS320F28062F-Q1 We use TMS320F28062F-Q1 control board to control a new delta connected permanent magnet synchronous motor. The motor parameters are :
Stator Resistance ( phase to phase ):5.6 m Ω; Stator Inductance (phase to phase )20 uH
M…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: TMS320F28062F , Hello,
I'm using C2000 series microcontroller TMS320F28062F. How can I program TMS320F28062F microcontroller using launchpad LAUNCHXL-F28069M ?
Regards,
Yusuf
Part Number: TMS320F28062F Other Parts Discussed in Thread: MOTORWARE
Hello TI: I have a complete motor control program in use. It was built many years ago with position sensor control. Recently there has been a need for a position sensorless solution…
Part Number: TMS320F28062F Hello TI:
I got a program from another engineer. I made some modifications but the test is abnormal. I want to use the emulator to debug. I found the following phenomenon when I opened the project settings.
The chip…
Part Number: TMS320F28062F Hi Guys,
I'm controlling a BLDC motor with 3phases which works perfectly.
In my case it could happen that, cause of user error, one of the 3 phases could disconnect. offcourse when having a disconnected phase the motor will…
Part Number: TMS320F28062F Other Parts Discussed in Thread: TMS320F28069F , MOTORWARE Tool/software: TI C/C++ Compiler Can the instaspin-foc module in tms320f28062f or tms320f28069f perform flux weakening control on IPM, and if so, how to implement it …