Part Number: TMS320F28067 Dear Shamim ,
Thanks for sharing information regarding SPRA902A , we are still facing issue in voltage and current loop control regarding taking gains and controller for resistive load i.e power varies from 100W to 1000W
for…
Part Number: TMS320F28067 Hello,
Does TI have any minimum current consumption data?
I am seeing big variations of the supply current during the initial flash programming (entered through bootloader SCI communication). Some of our applications inject…
Part Number: TMS320F28067 Hello,
I am able to reproduce the following situation:
I intentionally short circuit the CAN_HI and CAN_LO lines in order to generate a bus-off condition. Furthermore I run the following function every 62.5[us] out of a timer…
Part Number: TMS320F28067 Hello,
colleagues of mine identified that the CAN communication stops in a test setup at a random time with a TMS320F28067 processor. We connected to the non-communicating CPU via JTAG (without loading a new firmware image and…
Part Number: TMS320F28067 So....I have the CSM active. When I try to program new code on the DSP I get the error '10' (CSM locked) at flash erase.
The bootloader is located in flash sector A and it is copied in L3 DPSRAM (Secure Zone). The internal…
Part Number: TMS320F28067 Where can I find the reflow profile for the TMS320F28067?
I have been informed by an independent lab that my reflow process is causing delamination. How do I prevent that? What harm can it cause?
Part Number: TMS320F28067 Tool/software: Code Composer Studio I am having an issue with a project I'm building in CCS7.
when I build the exact same project in CCS5.5. It seems to be working just fine.
I'm using the same compiler version, xdctools…
Part Number: TMS320F28067 Hi Support,
Can you help me identifying the registers that are NOT returning to default value after a SW Reset issue? Is this valid also in case of "HW Reset" (by XRS pin)?
Thanks and regards,
Alberto
Part Number: TMS320F28067 Hi,
We faced one issue about ADC accuracy, the same configuration, with only one difference on register ADCINTSOCSEL2.
When ADCINTSOCSEL2=0, SOC8's accuracy is not good. When keeping the value ADCINTSOCSEL2 after offset calibration…
Part Number: TMS320F28067 Hi,
Customer has some questions about read/write of memory addresses:
1) If the code read an address, which is in "reversed" area, what will happen? For example the address is 0x3D7D00.
2) If the code read an address…