Part Number: TMS320F28069 Hello TI Team,
I am investigating a TMS320F28069 on a custom PCB that previously worked normally but can no longer be connected, erased, or programmed through JTAG.
I have two identical custom PCBs:
PCB-1: Working normally…
Part Number: TMS320F28069 Hi Team,
Iam using TMS320F28069 controller for my application. when iam using ADC perpheral, I found in TRM that ADC Clock is configured based on the "ADCCTL2" register configuration. If i set "CLKDIV4EN" & "CLKDIV2EN" bits…
Part Number: TMS320F28069 Other Parts Discussed in Thread: UNIFLASH , Dear TI,
We're using the TMS320F28069 in our products and are switching from development to production. Therefore, instead of a development password (key 4-7 custom, key 0-3 FFFF…
Part Number: TMS320F28069 Tool/software: What is the maximum frequency that can handled with the CPU Timers on the TMS320F28069?
Thank you in advance!
Sandy
Part Number: TMS320F28069 Hi,
I was wondering if there are any active powerline communication development kits that provide networking protocols such as G3?
Best,
PJ
Part Number: TMS320F28069 Hi, I want to update the firmware on my TMS320F28069 via CAN bus, since now I have been using a Debug probe or SCI (C2Prog app). I'm using the Stand-Alone Boot Mode, and so far I know, I need the pin TRST=0, then GPIO37 and GPIO34…
Part Number: TMS320F28069 Hi,
I'm trying to update the program on my processor through CAN boot mode. I have the CAN boot mode selected with GetMode, as indicated in the TRM.
I'm stucked transferring the program: after the Build of my project, the…
Part Number: TMS320F28069 Hi
We are using the OTP for our own bootup program. In the OTP memory section we write the following values to be able to boot in the OTP: 0x3D 7BFB OTP_KEY = 0x5A 0x3D 7BFE OTP_BMODE =0x06
Wyh the values between 0x3D7BFA…