Part Number: TMS320F2808 Tool/software: Hi All,
Customer is using SDFlash for flash writing. The device boots with SCI and assumes that the flash is written via RS232. SDFlash was available in Windows 10, but is no longer available in Windows 11. Is…
Part Number: TMS320F2808 Other Parts Discussed in Thread: C2000WARE Hi All,
is TMS320F2808 fixed point or floating point processor.?
If it is a fixed point, are there any libraries available for the floating point operations.
Thanks,
Pr…
Part Number: TMS320F2808 Hi,
we are using TMS320F2808 processor, we are working on Data loader code.
please provide for a reference if u have any sample data Loader source code sdk which supports the above mentioned processor
Thanks
Akhil.
Part Number: TMDSCNCD2808 Other Parts Discussed in Thread: C2000WARE , TMS320F2808 Tool/software: Unable to find hardware files/ examples at C2000Ware
TMDSCNCD2808 TMS320F2808 controlCARD
TI description says:
Features
TMS320F2808 Digital Signal…
Part Number: TMS320F2808
Tool/software:
When the F2808 is powered on, GPIO18, GPIO29, and GPIO34 are pulled up to enter the boot mode and ROM is started. If during this process of loading the program.Is the GPIO29 voltage suddenly low, causing the…
Part Number: TMS320F2808
In 'DSP280x_CpuTimers.c', the function below multiplies two 'float's, then casts the result to 'long', then lets assignment do the final cast to 'unsigned long' ... and am baffled by it. Is this a sign-extension idiom? (I almost…
Part Number: TMS320F2808 I would like to write my own custom bootloader for the F2808. I have never used a TI processor, and was wondering if you can do memory writes and jumps within code without issue? Basically, I was wanting to write the bootloader…
Part Number: TMS320F2808 Dear TI CSC,
I noticed that the maximum erase time written on the TMS320F2808 datasheet is 15 seconds, this parameter is for the first 100 erase/program cycles. But if we erase the IC for more than 100 cycles, what is the maximum…
Part Number: TMS320F2808 Hello, During microcontroller restart, GPIO CAN-Tx to ouput as seen in the attached photo, is floating and at microcontroller power on, jumps low and then quickly high at the program start. I want to instead, avoid this jumping…
Part Number: TMS320F2808 Hi,
I am using the military grade version of the TMS320F2808 micro-controller.
As part of a functional test in which the microcontroller is inside the housing, the only way for me to make changes to the microcontroller firmware…