Part Number: TMS320F28334 Other Parts Discussed in Thread: C2000WARE Hi,
In my code I am running my routine at 50us using ADC interrupt triggered using PWM. My code is related to AC induction motor control.
At every 50us adc interrupt is generated…
Part Number: TMS320F28334 Other Parts Discussed in Thread: C2000WARE , C2000WARE-MOTORCONTROL-SDK , CONTROLSUITE Hello,
I was checking HVACI_SENSORLESS_2833x example in CONTROL SUITE. In that Project I have doubts that I want to ask.
Which are as…
Part Number: TMS320F28334 Other Parts Discussed in Thread: CONTROLSUITE Hi,
I was understanding the HVACI_Sensorless_2833x example given at below path:
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVACI_Sensorless_2833x
I am not able…
Part Number: TMS320F28334 Other Parts Discussed in Thread: CONTROLSUITE Hi,
I am trying to control my ACI motor with the help of HVACI_Sensorless_2833x example given in controlsuite. currently I am testing Build Level 2.
Input Value in Build level…
Part Number: TMS320F28334 I am working on TMS320F28334 and i am configuring the TRIP signal event for ePWM1A and ePWM1B. During the trip signal event i will enable bits such that ePWM1A will go low and ePWM1B will go high .
The question is which of…
Part Number: TMS320F28334
Hi,
In code composer studio , I am taking some data in my code in an array. I want that array to export in Excel file to See its Graph. Is there any Option in Code composer studio to export it in excel?
Currently I am select…
Part Number: TMS320F28334
Imagine i configured the ePWM1A and configured ePWM1B be complimentary of ePWM1A.
Question 1
if i set the bits such that during Trip Signal event ePWM1A pin to be low. what would be state of ePWM1B pin during trip signal…
Part Number: TMS320F28334
Hello,
I am using TMS320F28334, the connection for JTAG are as per image shared below which is given in the technical documentation for the given MCU.
I am facing problem in which uploading the code. I am using TMS320…
Part Number: TMS320F28334 Other Parts Discussed in Thread: C2000WARE Hi All, What is the difference between below 2 functions in IQ math lib. 1.) _IQ(2.0);
2.) _IQ2toIQ(2.0); Also, Please elaborate when to use function 1 and function 2 with an individual…
Part Number: TMS320F28334 I am using a FT2232D USB Interface to program the flash on the on-board TMS320F28334. I can connect using CCS on my laptop but get an error when using another computer.
The message is:
Error connecting to the target
Error…